Skip to main content

Create Images and Flash

Before you begin, following are parameter descriptions:
Base on your modules, select the <board-name>.

Product name<board-name>Boot device
TEK6100-ORIN-NXtn-tek6100-orinNVMe/ USB
TEK6040-ORIN-NANOtn-tek6040-orinNVMe/ USB

Base on your condition, select the <rootdev>.

Boot device<rootdev>
NVMenvme0n1p1
USBsda1

<board-name> : specifies the configuration of the target device.
<rootdev> : specifies the device on which the root file system is located.


Enter Recovery Mode

When it comes to using 'flash.sh', make sure you enter the Recovery mode first.

  1. Connect to computer via M-USB1.
  2. Plug the storage you want to flash system image.
  3. Press 'Recovery' button and 'Reset' button at the same time.
  4. Release 'Reset' button.
  5. Release 'Recovery' button.
  6. Check wether the device is connected.
    $ lsusb
    Bus 003 Device 026: ID 0955:7323 NVIDIA Corp. APX

Prepare JetPack host environment

Please follow host environment setting to download codebase and compile images.

You are ready

When you prepare JetPack, the download script will create system.img,
you can flash into device directly.

Flash on Recovery Mode

Flash options

$ cd <nvidia_folder>
$ ./technexion_jetpack_download.sh -b <board-name> <flash_option>

<flash_option> : support the following flash options

Example: build system.img and flash into TEK6100-ORIN-NX

$ ./technexion_jetpack_download.sh -b TEK6100-ORIN-NX --build-flash

Flash using Nvidia script for ORIN series
Run this command from the Linux_for_Tegra folder:

$ cd <nvidia_folder>/Linux_for_Tegra/
$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh <option> <board-name> <rootdev>

<option> : is one or more command line options for flash.sh script.

DO NOT create new system.img, flash only

You can follow section: Create new system.img, DO NOT flash to create system.img.

# use '--flash-only' option
$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--external-device <rootdev> -c tools/kernel_flash/flash_l4t_external.xml \
-p "-c bootloader/generic/cfg/flash_t234_qspi.xml" \
--showlogs --flash-only --network usb0 <board-name> internal

Example: flash TEK6100-ORIN-NX with NVMe boot device.

$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--external-device nvme0n1p1 -c tools/kernel_flash/flash_l4t_external.xml \
-p "-c bootloader/generic/cfg/flash_t234_qspi.xml" \
--showlogs --flash-only --network usb0 tn-tek6100-orin-nx internal
--flash-only limitation

JetPack stores the command that you previously used to create system image
in bootloader/flashcmd.txt
Example1: TEK6100-ORIN-NX: NVMe boot

./tegraflash.py ...
bpmp_fw bpmp_t234-TE980M-A1_prod_sigheader.bin.encrypt;
bpmp_fw_dtb tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt;
kernel_dtb tegra234-tek-orin+p3767-0000-nv.dtb
...

Example2: TEK6040-ORIN-NANO: NVMe boot

./tegraflash.py ...
bpmp_fw bpmp_t234-TE950M-A1_prod_sigheader.bin.encrypt;
bpmp_fw_dtb tegra234-bpmp-3767-0001-3509-a02_with_odm_sigheader.dtb.encrypt;
kernel_dtb tegra234-tek-orin+p3767-0003-nv.dtb
...

Most of the differences can be found in their board conf file.


In conclusion, when running --flash-only command, if the <rootdev> or <board-name> does not match the previously created one, flash script will be terminated.

When any of them changes, need to create system.img again.
Or you can just create new JetPack with different system image command.


Create new system.img, and flash

$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--external-device <rootdev> -c tools/kernel_flash/flash_l4t_external.xml \
-p "-c bootloader/generic/cfg/flash_t234_qspi.xml" \
--showlogs --network usb0 <board-name> internal

Create new system.img, DO NOT flash

You are ready

When you prepare JetPack, download script will create system.img,
you can flash into device directly.

# use `--no-flash` option
$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--external-device <rootdev> -c tools/kernel_flash/flash_l4t_external.xml \
-p "-c bootloader/generic/cfg/flash_t234_qspi.xml" \
--showlogs --no-flash --network usb0 <board-name> internal

You can flash to device following section: DO NOT create new system.img, flash only.



Create disk image and flash

You also can create disk image for flashing into external storage.

  1. Run below commmand to

    $ cd <nvidia_folder>/Linux_for_Tegra/
    $ sudo ./tools/jetson-disk-image-creator.sh -o <output-img> -b <board-name> -d <rootdev>

    For example:
    sudo ./tools/jetson-disk-image-creator.sh -o TEK6100_nvme.img -b tn-tek6100-orin-nx -d NVMe
    This command will create a TEK6100_nvme.img. Could be dd into storage.

  2. Generate bmaptool files

    $ sudo bmaptool create <output-img> -o <output-img>.bmap
    $ sudo bzip2 -z <output-img>
  3. Connect the storage to computer and flash to block device

    # get your storage block device, it maybe shown sdX
    $ lsblk -d
    sdb 8:16 0 232.9G 0 disk

    # umount block device. Based on above example, <BLOCK_DEVICE> is sdb
    $ sudo umount /dev/<BLOCK_DEVICE>?

    # flash demo image into block device
    $ sudo bmaptool copy <output-img>.bz2 /dev/<BLOCK_DEVICE>
    NVMe storage

    We recommend using 'SSD Enclosure Adapter' to transform NVMe SSD to USB block device.

  4. Plug the storage back to device and boot.

    Multiple storage connected

    Make sure you select the right boot device in NVIDIA UEFI stage.


Create QSPI image

After JetPack 6, we can use generate_qspi_for_flash.sh to create QSPI image.

BE CAREFUL!!

When you upgrade UEFI firmware to JetPack 6(R36.4.ga), you CAN NOT downgrade to JetPack 5(R35.3.ga) quickly.
If you need to downgrade to JetPack 5, please download JetPack 5 SDK then compile and build QSPI image.


  1. generate qspi package

    $ cd <nvidia_folder>/Linux_for_Tegra/
    $ sudo ./tools/qspi_flash/generate_qspi_for_flash.sh <board-name>

    The output file is host_tegraflash_${VERSION}.tbz2.
    ${VERSION} is R36.4.3 for JetPack 6.2.

  2. Device enter to recovery mode

  3. unzip host_tegraflash_${VERSION}.tbz2 and flash

    $ tar -xvf host_tegraflash_${VERSION}.tbz2
    $ sudo hostflash/host_flash_qspi.sh


Flash new pinmux image

  1. Edit the xlsm pinmux file via windows environment. TechNexion source file:

    <nvidia_folder>/Linux_for_Tegra/sources/TEK-ORIN_Orin-Nano_pinmux/Jetson_Orin_NX_and_Orin_Nano_series_Pinmux_Config_Template.xlsm
    ORIN-EVK

    Download xlsm pinmux file from NVIDIA server.

    pinmux1.png

    Use the scroll bar right to select the pinmux of the cell(pin).

    watch out the sheet
    • You should work on HDMI sheet, there are slightly different between them.
    • Please enable macro before you edit pinmux table.

    If done, click the above Macro(Generate DT file) to generate pinmux file.

    image(67).png

  2. Type the <name> twice. tek-orin-a1 for TEK-ORIN series image(68).png

    You will see this result. image(71).png There are 3 dtsi files generated.

  3. Copy generated dtsi to bootloader/ folder

    $ sudo cp -rp Orin-tek-orin-a1-gpio-default.dtsi Linux_for_Tegra/bootloader/
    $ sudo cp -rp Orin-tek-orin-a1-pinmux.dtsi Linux_for_Tegra/bootloader/generic/BCT/
  4. Update NVIDIA QSPI for pinmux follow the Create and flash new QSPI image only.



Those only update by file system

Protect the boot flow for saving your time.

You may want to see this article before you changing files.

Those part below can't be changed by flash.sh. Need to change the file by:

  1. ssh (scp)
  2. USB stick

Update new kernel Image

Copy from:

<nvidia_folder>/Linux_for_Tegra/source/kernel_out/kernel/kernel-jammy-src/arch/arm64/boot/Image

to device:

/boot/

Update new kernel modules

Copy from

<nvidia_folder>/Linux_for_Tegra/rootfs/usr/lib/modules/

to device:

/lib/

Update device tree

From:

<nvidia_folder>/Linux_for_Tegra/source/kernel_out/kernel-devicetree/generic-dts/dtbs/<target>.dtb

to device:

/boot/<target>.dtb

Change default device-tree

On device:

$ vi /boot/extlinux/extlinux.conf
LABEL primary
MENU LABEL primary kernel
+ FDT /boot/<target>.dtb
LINUX /boot/Image
INITRD /boot/initrd
APPEND ${cbootargs} root=/dev/mmcblk0p1 rw rootwait rootfstype=ext4 console=ttyTCU0,115200n8 console=tty0 fbcon=map:0 net.ifnames=0