Skip to main content

Host Environment Setting

Prepare ubuntu computer

Ubuntu 22.04.4 LTS (Jammy Jellyfish) is recommended.
You can also use ubuntu virtual machine.

Create workspace

Create and enter the nvidia workspace folder

$ mkdir <nvidia_folder> && cd <nvidia_folder>

Download the TN-JetPack using the download script

Get the download script

  1. Go to TechNexion Jetson JetPack script github
    Select tn_l4t-r36.4.ga_kernel-5.15 branch. JP62-github-branch.png

  2. Click the '< > Code' button image(61).png

  3. Copy the URL of HTTPS Or using SSH if match the requirement.

  4. Using git command to download the script and named 'download_script'

    $ git clone <URL> -b tn_l4t-r36.4.ga_kernel-5.15 download_script
    Cloning into 'download_script'...
    remote: Enumerating objects: 186, done.
    remote: Counting objects: 100% (101/101), done.
    remote: Compressing objects: 100% (64/64), done.
    remote: Total 186 (delta 63), reused 71 (delta 37), pack-reused 85
    Receiving objects: 100% (186/186), 49.06 KiB | 1.63 MiB/s, done.
    Resolving deltas: 100% (107/107), done.

Run the download script

  1. Make sure you are at correct branch

    $ git branch
    * tn_l4t-r36.4.ga_kernel-5.15
  2. copy the script and board conf to nvidia workspace folder (current folder)

    $ pwd
    <nvidia_folder>
    $ cp -rv download_script/technexion_jetpack_download.sh ./
    $ cp -rv download_script/*.conf ./
  3. Run script and wait for complete
    You must enter the required option to make it start.

    ./technexion_jetpack_download.sh
    download the Technexion JetPack -b <baseboard>
    -b: baseboard <TEK6040-ORIN-NANO/ TEK6100-ORIN-NX>

    Jetson Orin series:
    TEK6040-ORIN-NANO| TEK6100-ORIN-NX

    -t: tag for sync code <>

    --qspi-only: do not create/flash rootfs, for QSPI image only
    example
    $ ./technexion_jetpack_download.sh -b TEK6100-ORIN-NX

    You can set and switch to certain tag using -t <tag name>

    Tag chart
    tag nametag description
    r36.4.gaTechNexion SW with JetPack 6.2.0 Nvidia L4T 36.4.3

    example:

    $ ./technexion_jetpack_download.sh -b TEK6100-ORIN-NX -t r36.4.ga

Once it done, this folder will contain:

  • TechNexion camera source code
  • Device-tree of TechNexion product
  • Modified NVIDIA kernel
  • Bootable system image that ready to be deployed into device.

system image must be the default storage type.
TEK-ORIN series: NVMe
ORIN-EVK series: SD

Troubleshooting

  • You might need to enter the sudo password twice if the script takes too much time.
  • Script will exit if it gets any error, and you will see the error description on console.