Some Debug Tips Before You Start
Add another boot config
We highly recommend you to add another boot config for it.
So when you make a mistake, you can boot using another boot config.
(Re-creating system.img or flashing the entire system image takes a lot of time.)
And rename your test file before you copy into target folder.
$ vi /boot/extlinux/extlinux.conf
LABEL primary
MENU LABEL primary kernel
LINUX /boot/Image
INITRD /boot/initrd
FDT /boot/<target>.dtb
APPEND ${cbootargs} ...
+ LABEL TEST_KERNEL
+ MENU LABEL TEST kernel
+ LINUX /boot/Image_test
+ INITRD /boot/initrd
+ FDT /boot/<target>_test.dtb
+ APPEND ${cbootargs} ...
When booting to UEFI, follow the step to change boot device.
Or you can select the TEST_KERNEL boot config by typing '2' in console.
Boot from USB stick
Another way for safety boot is using USB stick boot.
Follow section: Flash demo image to create new USB boot device, when boot to UEFI select the right boot device.
If you follow the section: Create new system.img, and flash to create a USB boot device, make sure you modify the /boot/extlinux/extlinux.conf
- root=PARTUUID=ad43ec6f-6d79-4df0-b915-1c936b0e33ef
+ root=/dev/sda1
Otherwise, the OS might select the wrong rootfs device.
Go to this website for more detail.
Remove/ modify the default user and password
In download script, we add a default user ubuntu:ubuntu
# vim technexion_jetpack_download.sh #Line: 274
# create default user and auto login
sudo Linux_for_Tegra/tools/l4t_create_default_user.sh -u ubuntu -p ubuntu -a
# -a stands for auto login.
This user can't be removed, so remove/ modify this line BEFORE you run the download script.