Host Environment Setting
Prepare ubuntu computer
Ubuntu 22.04.4 LTS (Jammy Jellyfish) is recommended.
You can also use ubuntu virtual machine.
Create workspace
Create and enter the nvidia workspace folder
$ mkdir <nvidia_folder> && cd <nvidia_folder>
Download the TN-JetPack using the download script
Get the download script
-
Click the '< > Code' button
-2d709b7fa4fc28cb39852ee754ea67ca.png)
-
Copy the URL of HTTPS Or using SSH if match the requirement.
-
Using git command to download the script and named 'download_script'
$ git clone <URL> download_script
Cloning into 'download_script'...
remote: Enumerating objects: 186, done.
remote: Counting objects: 100% (101/101), done.
remote: Compressing objects: 100% (64/64), done.
remote: Total 186 (delta 63), reused 71 (delta 37), pack-reused 85
Receiving objects: 100% (186/186), 49.06 KiB | 1.63 MiB/s, done.
Resolving deltas: 100% (107/107), done.
Run the download script
- change the permission of the script
$ chmod a+x download_script/technexion_jetpack_download.sh
- copy the script and board conf to nvidia workspace folder (current folder)
$ pwd
<nvidia_folder>
$ cp -rv download_script/technexion_jetpack_download.sh ./
$ cp -rv download_script/*.conf ./
- Run script and wait for complete You must enter the required option to make it start.
./technexion_jetpack_download.sh
download the Technexion JetPack -b <baseboard>
-b: baseboard <TEK6020-ORIN-NANO/ TEK6040-ORIN-NANO/ TEK6070-ORIN-NX/ TEK6100-ORIN-NX
TEV-RPI22-TEVI/ TEV-RPI22-TEVS/ VLS3-ORIN-EVK-VLS3/ VLS3-ORIN-EVK-VLI>
Jetson Orin series:
TEK6020-ORIN-NANO| TEK6040-ORIN-NANO| TEK6070-ORIN-NX| TEK6100-ORIN-NX
Jetson Orin EVK series:
TEV-RPI22-TEVI| TEV-RPI22-TEVS| VLS3-ORIN-EVK-VLS3| VLS3-ORIN-EVK-VLI
-t: tag for sync code <>
--qspi-only: do not create/flash rootfs, for QSPI image only
example
$ ./technexion_jetpack_download.sh -b TEK6100-ORIN-NX
$ ./technexion_jetpack_download.sh -b VLS3-ORIN-EVK-VLS3
You can set and switch to certain tag using -t <tag name>
Tag chart
| tag name | tag description |
|---|---|
| r35.3.ga | TechNexion SW with JetPack 5.1.1 Nvidia L4T 35.3.1 |
example:
$ ./technexion_jetpack_download.sh -b VLS3-ORIN-EVK-VLS3 -t r35.3.ga
Once it done, this folder will contain:
- TechNexion camera source code
- Device-tree of TechNexion product
- Modified NVIDIA kernel
- Bootable system image that ready to be deployed into device.
system image must be the default storage type.
TEK-ORIN series: NVMe
ORIN-EVK series: SD
Troubleshooting
- You might need to enter the sudo password twice if the script takes too much time.
- Script will exit if it gets any error, and you will see the error description on console.
-d3876d47e30a454622c32dec4d9ee1fd.png)