Skip to main content

Flash Demo Image

Flash demo image steps

  1. Download TechNextion demo image:

    ProductDemo image
    TEK6100-ORIN-NXNVMe TEK6100-ORIN-NX_JP6_ubuntu-22.04_hdmi_NVMe_diskimg.zip
    USB TEK6100-ORIN-NX_JP6_ubuntu-22.04_hdmi_USB_diskimg.zip

    Make sure you download the image with the boot device you need.

  2. Unzip the zip file
    You will get 3 files likes below:

    • Procuct_storage_disk.img.bz2
    • Procuct_storage_disk.img.bmap
    • Product_hostflash.tbz2
  3. Connect the storage to computer and flash to block device

    # get your storage block device, it maybe shown sdX
    $ lsblk -d
    sdb 8:16 0 232.9G 0 disk

    # umount block device. Based on above example, <BLOCK_DEVICE> is sdb
    $ sudo umount /dev/<BLOCK_DEVICE>?

    # flash demo image into block device
    $ sudo bmaptool copy <FILE.bz2> /dev/<BLOCK_DEVICE>
    NVMe storage

    We recommand using 'SSD Enclosure Adapter' to transform NVMe SSD to USB block device.

  4. Plug the storage back to device and boot.

    Multiple storage connected

    Make sure you select the right boot device in NVIDIA UEFI stage.


Update UEFI firmware

When Jetpack version is changed or modify kernel, you also need to update UEFI firmware.
If UEFI firmware and system image is not matched, device can't boot up.
Please refer Update UEFI firmware from demo image