Create Custom Bootable system.img
Demo image (system.img)
There are two steps to do:
- Prepare files
- Create system.img
1. Prepare files
- kernel Image
- kernel modules
- kernel dts
- pinmux
- change boot config for custom device-tree(overlay)
kernel Image
Copy from:
<nvidia_folder>/Linux_for_Tegra/sources/kernel/kernel-5.10/arch/arm64/boot/Image
to here
<nvidia_folder>/Linux_for_Tegra/kernel/
kernel modules
Copy from
<nvidia_folder>/Linux_for_Tegra/sources/kernel/modules/lib/
to here
<nvidia_folder>/Linux_for_Tegra/rootfs/
rootfs files
Copy anything you want to deploy to image to here
<nvidia_folder>/Linux_for_Tegra/rootfs/
device-tree
Copy from
<nvidia_folder>/Linux_for_Tegra/sources/kernel/kernel-5.10/arch/arm64/boot/dts/<target>.dtb
to here
<nvidia_folder>/Linux_for_Tegra/rootfs/boot/<target>.dtb
pinmux (TEK-ORIN series for example)
Copy
Orin-tek-orin-a1-gpio-default.dtsi
to here
<nvidia_folder>/Linux_for_Tegra/bootloader/
Copy
Orin-tek-orin-a1-pinmux.dtsi
to here
<nvidia_folder>/Linux_for_Tegra/bootloader/t186ref/BCT/
For Orin-EVK pinmux
Remember, ORIN-EVK series has different pinmux file name.
Please rename it.
<SOM>-<board_name >-gpio-default.dtsi
-> tegra234-mb1-bct-gpio-p3767-dp-a03.dtsi
<SOM>-<board_name >-pinmux.dtsi
-> tegra234-mb1-bct-pinmux-p3767-dp-a03.dtsi
boot config for custom device-tree
<nvidia_folder>/Linux_for_Tegra/rootfs/boot/extlinux/extlinux.conf
LABEL primary
MENU LABEL primary kernel
LINUX /boot/Image
INITRD /boot/initrd
+ FDT /boot/<target>.dtb
- APPEND ${cbootargs} quiet
+ APPEND ${cbootargs}
2-1. Create system.img
Follow Flash Step section: Create new system.img, DO NOT flash.
2-2. Create raw system.img that can be dd'd into storage
Follow Flash Step section: Flash demo image.