Skip to main content

Usage Guide


Overview​


Enumerate and List All Video Devices​

When VizionViewer™ starts, it displays an initial screen showing all available video devices. You can select a camera either from this device list or from the dropdown menu. The device list refreshes every second.

Camera Selection


Change Streaming Format​

Color Space / Compression​

After selecting a camera, the color space/compression dropdown displays all supported formats. Supported formats include UYVY, YUY2, NV12, and MJPG.

Resolution​

Once a color space/compression is chosen, the resolution dropdown lists all supported resolutions for the selected camera.

Framerate​

After selecting a resolution, the framerate dropdown displays all supported framerates.


Display the Current Frame Rate Per Second​

info

"Stream Frame Rate" refers to the camera's streaming output rate, not the rendering rate of VizionViewer™.

Frame Rate Display


Extension Settings Control​

info

Switching the Control Mode to UVC will reset ISP Extension settings to default. Switching to ISP mode will reset UVC Extension settings to default.

Extension Controls

UVC Mode Extensions​

Supported controls:

  • White Balance (Auto / Manual)
  • Exposure / Gain (Auto / Manual)
  • Contrast
  • Saturation
  • Sharpness
  • Gamma
  • Brightness
  • Hue
  • Backlight
  • Focus
  • Iris
  • Zoom
  • Pan
  • Tilt
  • Roll

ISP Mode Extensions​

White Balance (Auto / Manual)​

EHDR Settings (Note: Supported only on device models 0821 and 0822)​

  • State: Enable / Disable
  • Exposure: Set Min/Max Number
  • Ratio: Set Min/Max Ratio

Exposure / Gain (Auto / AGC / Manual)​

Image Adjustment​

Supported controls:

  • Contrast
  • Saturation
  • Sharpness
  • Denoise
  • Backlight Compensation
  • Brightness
  • JPEG Quality
  • Filter: Apply visual effects (Black and White, Grayscale, Negative, Sketch)
  • Flick Mode: Reduce flickering under artificial lighting (Disable, 50Hz, 60Hz, Auto)

Region of Interest​

Control the camera's field of view:

  • Zoom: Adjust the zoom level
  • Pan: Move the view horizontally
  • Tilt: Move the view vertically
  • Flip Mode: Rotate or mirror the image (Vertical, Horizontal, Rotate 180°)

Set Up AGC Exposure Mode to Maintain Constant Framerate​

Floating Framerate

For low-light applications, the camera increases exposure time in automatic exposure mode to maintain image quality.

You can switch to AGC exposure mode to keep the framerate constant.

AGC Mode

Auto gain control, manual exposure time.

When AGC mode is enabled, gain is set automatically. The initial exposure value adjusts based on the current streaming framerate to maintain a constant framerate.

AGC Mode


Limit Exposure Range in Auto Exposure Mode​

(Default Exposure Range) When switching to Auto Exposure Mode, the Exposure Time Range is automatically set to the default range based on the selected streaming format.

You can limit the exposure range even in Auto Exposure Mode. This is useful when you want to avoid overexposure or motion blur in specific lighting conditions. The default exposure range varies depending on the selected resolution and framerate.

The current Exposure Time and Exposure Gain values are displayed after the camera starts streaming and are updated every second to reflect real-time changes.

Exposure Range


Update Technexion Camera Firmware​

If firmware updates are available for the selected camera, the Update button becomes enabled. You can:

  • Update your camera's firmware directly
  • Download firmware for later installation

Firmware Update Download for Later


Recondition Tool​

The Recondition Tool restores UVC cameras to factory settings — useful when a camera is misconfigured, unresponsive, or needs to be redeployed. It also supports serdes cameras via single-port USB serdes framegrabbers. Open it from the Recondition Tool button in the Firmware Information section.

Recondition Tool Button Recondition Tool

Verify the Camera Series Before Reconditioning​

The detected series may be incorrect in recovery mode

If the wrong firmware was previously installed, the camera may be detected as a different series. Treat the option marked (detected) as a suggestion, not a guarantee.

Before clicking Recondition Firmware:

  1. Check the model printed on the camera label or the original order information.
  2. Select the series that matches the camera's original product model.
  3. Connect only one camera and confirm the selection before continuing.

For example, if a VC, VCS, or VCM camera is shown as VC-UnknownBoot or VCI-UnknownBoot, select VC (VCS / VCM Recovery). Select VCI only if the original product is a VCI camera.

If you are unsure which series to select, stop and contact TechNexion Support before continuing. Selecting the wrong series may cause recovery to fail or install the wrong firmware again.

Select the camera's original series before reconditioning

Supported Cameras​

SensorUSB3 (VCI)USB3 (VCS, VCM)USB to FPD-Link III Frame Grabber (UVC-VLS-FPD3)USB to GMSL2 Frame Grabber (UVC-VLS-GM2, UVC-VLM-GM2)
AR0144✓✓✓✓
AR0145✓✓✓
AR0234✓✓✓✓
AR0235✓✓
AR0246✓✓
AR0521✓✓✓✓
AR0522✓✓✓✓
AR0544✓✓
AR0821✓✓✓✓
AR0822✓✓✓✓
AR0830✓✓
AR1335✓✓✓✓
AR2020✓✓

Manage OS Profiles​

Profiles allow you to save video stream and extension settings for your camera. You can create and name multiple profiles for different scenarios, making it easy to apply predefined configurations.

OS Profile Management

#ItemDescription
①Profile NameThe name assigned to this configuration profile.
②ModifyClick to edit the profile name.
③Dropdown listList all profiles on the local platform that match this sensor.
④Set as OSPActivates and saves the profile, then copies it to OSP. The button can only be pressed when camera is streaming.
⑤AddCreates a new configuration profile.
⑥DeleteDeletes the currently selected configuration profile.
⑦ActivateEnables the selected configuration profile.
⑧SaveSaves the currently selected configuration profile.

Manage OSP (On Sensor Profile)​

Store profiles directly on the sensor. The camera will automatically apply your preset profile upon startup.

OSP Profile Settings

#ItemDescription
①Profile NameThe name assigned to this configuration profile. Default as OSP_{last5 characters of uid}
②ModifyClick to edit the profile name.
③Set as ProfileActivate and save the OSP setting, then create a new profile and copy the configuration for storage. If a profile with the same name already exists, it will be overwritten.
④ActivateEnables the OSP profile.
⑤SaveSaves the currently modified settings.
⑥ClearReverts all unsaved changes.

Install Camera Drivers Online​

The Camera Driver Installer detects the current system and installs a compatible camera driver from the online catalog. Use it to prepare a supported platform for a MIPI CSI-2 or GMSL camera that requires a platform-specific driver.

Before installing

Installing a camera driver changes system-level files and requires administrator authentication. Back up important system customizations, keep the device powered, and make sure it has a stable internet connection.

Open the Camera Driver Installer​

  1. Open Labs (beta).
  2. In the Camera Driver (beta) panel, click Camera Driver Installer.

Open the Camera Driver Installer from Labs

The dialog displays the detected platform, kernel, architecture, and support status. It also shows the platforms available in the current online catalog. In the example below, NVIDIA Jetson developer kits, supported third-party Jetson systems, Raspberry Pi 4, and Raspberry Pi 5 are available. The same high-level installation flow applies to NVIDIA Jetson and Raspberry Pi.

Detected system and supported camera-driver platforms

For NVIDIA Jetson, use the information icons to see the Jetson developer kits and third-party systems supported by the current catalog. The list can change as new driver packages are published. Platforms under Coming Soon cannot be installed from VizionViewer™ yet.

Supported third-party NVIDIA Jetson systems

Select and Install the Driver​

The following example installs the driver for a VLS-GM2 GMSL2 camera on an NVIDIA Jetson AGX Orin Developer Kit:

  1. Click Install after the detected system shows Supported.
  2. Select the Platform category, Platform model, and Camera module.
  3. Check the detected L4T version and Install availability. If a compatible release is available, click Confirm.

Select a compatible NVIDIA camera driver

  1. When the system asks for authentication, enter the password for the shown administrator account and click Authenticate.

Authorize camera-driver installation

VizionViewer™ downloads the selected package and displays the installer output in Installation Log. Do not close VizionViewer™ or power off the system while the installer is running. If support assistance is needed, click Export to save the log.

Reboot and Verify the Camera​

After Installation succeeded appears, reboot the system to apply the driver. Click Reboot to restart immediately, or Later to restart manually.

Reboot after camera-driver installation succeeds

After the system restarts, open VizionViewer™ and check Camera Selection. The connected cameras should now be listed.

Cameras detected after installing the driver and rebooting

Select a camera and start streaming to confirm that frames can be captured. Camera detection confirms that the driver can enumerate the device; a successful preview confirms end-to-end streaming.


GMSL Margin Test​

Measures the forward (DES) and reverse (SER) link margin to verify signal integrity between the serializer and deserializer.

GMSL Test Button

Click the button to open the test dialog, select the number of iterations (1–3), then click Run to start the test.

GMSL Test

Result Example

GMSL Test Result


Preview Features​

Grid Overlay​

Grid

Display composition guides on the camera preview to help with framing and alignment. Choose from multiple grid types:

  • Off: No grid overlay
  • Rule of Thirds: Classic 3×3 grid for balanced composition
  • Golden Ratio: Grid based on the golden ratio for aesthetic framing
  • Crosshairs: Center cross for precise alignment
  • Square: Centered square guide

IMU 3D Preview​

info

This feature is only available on VCM/TEVM cameras.

  • Enable IMU 3D Preview: Click the button to enable the feature

IMU 3D Preview

  • Reset Model: Click 'Reset' to reset the preview model display to origin (camera IMU data remains unchanged) IMU 3D Preview Reset

  • IMU Data Display: Cick ‘Data’ to show live imu data stream

IMU 3D Preview Data

  • PIP IMU Data: Click ‘PIP’ button to make IMU data PIP

IMU 3D Preview PIP


Record Videos and Capture Photos​

Record Videos​

info

On embedded platforms, the maximum recording resolution is 1920x1200.

  • Video Codec Options: Choose between H264 (compressed, smaller file size) or FFV1 (lossless, larger file size)
  • Filenames follow the format: yyyyMMdd_hh_mm_ss_zzz.avi
  • Default storage location: system default path (Tools → File → Open Video Folder)
  • To change codec or storage location: Tools → File → Options

Take Photos​

  • Image Format Options: Choose from BMP, PNG, JPG, or Direct Buffer (raw)
  • Filenames follow the format: yyyyMMdd_hh_mm_ss_zzz.[format]
  • Default storage location: system default path (Tools → File → Open Image Folder)
  • To change format or storage location: Tools → File → Options

Stream Format Preference​

Configure your preferred camera stream format for optimal performance:

  • YUY2: Packed YUV 4:2:2 format, good quality with moderate bandwidth
  • UYVY: Packed YUV 4:2:2 format, similar to YUY2 with different byte order
  • NV12: Planar YUV 4:2:0 format, efficient for video processing
  • MJPEG: Motion JPEG format, compressed with lower bandwidth usage

Access these settings through Tools → File → Options.


Camera Simulation​

  • View multiple cameras simultaneously: Observe up to eight camera feeds at once.
  • Stream All / Stop All: Quickly start or stop streaming for all cameras at once with convenient control buttons.

Camera Simulation Stream All


Route Configuration (IMX93/95 Users)​

For i.MX93 and i.MX95 platforms, you can load route configuration files to automatically set up camera media links. This feature enables the correct MIPI or GMSL camera connections for your system.

Route Config Button Route Config

To load a route configuration:

  1. Click the route configuration button
  2. Select the appropriate YAML configuration file for your camera setup
  3. Click Activate to apply the configuration

The system will automatically configure the media links based on the selected route configuration file.

See more: Camera Media Route Configuration​


Customize Layout with Drag-and-Drop​

Layout Customization​

Drag panel title bars to reposition interface elements.

Drag Layout


Change Color Theme​

Select theme from Tools → Settings → Appearance (Ocean Blue/Dream Purple/Mountain Green).

Color Theme


Logo Options​

  • Default Logo: TechNexion branding
  • Hide Logo: No logo displayed
  • Custom Text Logo: Enter custom text
  • Custom Image Logo: Upload SVG image file

Configuration​

  • Access: App Settings -> Customize Logo
  • Select logo type
  • For Custom Image Logo: Browse and select file
    • Supported formats: SVG
    • Recommended size: 206×26 pixels (SVG with transparent background)

Custom Logo


Export Log Files​

VizionViewer™ records its activity, including camera discovery, streaming, firmware updates, and Recondition Tool operations, in a log file. When you report an issue, the log file helps TechNexion Support find the cause.

Reproduce the issue first

Export the log right after the issue occurs, without restarting VizionViewer™ in between. If you are reporting a Recondition Tool failure, run the reconditioning once, close the Recondition Tool after the error appears, and then export the log. When several cameras are affected, export one log per camera and note each camera's serial number.

  1. Open the Tools tab.

  2. In the File section, click Export Log File.

    Export Log File in the File section

  3. In the Export Log Files dialog, check that the log files are listed under Log Files Found.

  4. Click Browse to choose a Location, and change the File Name if needed. The default name includes the export date and time, for example VizionViewer_logs_2026-10-12T16-57-36.zip.

  5. Click Export. VizionViewer™ saves all listed log files in a single .zip file.

    Export Log Files dialog

If VizionViewer™ cannot start

You can collect the log files manually from the log folder:

PlatformLog folder
Windows%APPDATA%\TechNexion Ltd\VizionViewer\VizionViewer\logs
Linux~/.local/share/VizionViewer/linux/logs
eLinux~/.local/share/VizionViewer/elinux/logs

On Windows, paste the path into the File Explorer address bar to open the folder.


Support​

If you encounter any issues with VizionViewer™:

  1. Export the log files right after the issue occurs.
  2. Describe the issue, including the camera model, serial number, operating system, and the steps that lead to the issue.
  3. Attach the exported .zip file and any screenshots of error messages.
  4. Send everything to support.vision@technexion.com.