Release Notes
v26.10.1
Release Date: 2026-10-28
Updated
- Factory Recondition Tool: Separated the Factory Recondition Tool from Firmware Update into a standalone recovery feature.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.09.1
Release Date: 2026-8-28
Added
- Factory Recondition Tool: Added a camera series verification warning and a dedicated VC (VCS / VCM Recovery) option for cameras detected in
VC-UnknownBootrecovery mode. - TI/Yocto Support: Added IPK packages for installation on supported TI/Yocto systems.
Updated
- Camera Workspace: Improved camera workspace layout and control responsiveness.
Fixed
- Factory Recondition Tool: Fixed the recovery path for VCS and VCM cameras detected in
VC-UnknownBootmode. - Fixed various minor bugs and improved overall stability.
Download
v26.08.1
Release Date: 2026-8-20
Added
- TI/Yocto Support: Added IPK packages for installation on supported TI/Yocto systems.
Updated
- Camera Workspace: Improved camera workspace layout and control responsiveness.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.07.2
Release Date: 2026-7-15
Added
- In-App Logger: Added an in-app log panel to help users troubleshoot and diagnose issues.
Updated
- User Interface: Improved the overall UI and user experience.
Fixed
- Simulation: Fixed an issue when applying the same configuration to all existing cameras of the same model.
Download
v26.07.1
Release Date: 2026-7-9
Added
- Camera Driver (Beta): Integrated the previous NVIDIA Camera Driver and Raspberry Pi Camera Driver into a single camera driver workflow. The application now automatically detects the environment and selects the appropriate driver.
- Simulation: Added support for applying the same configuration to all cameras of the same type with one click.
Updated
- Multi-Firmwares Update (Beta): Firmware updates for multiple components can now run concurrently instead of sequentially.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.05.1
Release Date: 2026-5-12
Added
- Labs Tab: Added a new Labs tab for experimental and preview features.
- NVIDIA Camera Driver Support (Beta): Added beta support for installing and managing NVIDIA camera drivers directly within the application.
- Raspberry Pi Camera Driver Support (Beta): Added beta support for Raspberry Pi camera driver installation and configuration.
- Multi-Firmwares Update (Beta): Added beta support for updating multiple firmware components in a single workflow.
Updated
- GMSL Link Margin Tool: Improved the user interface and overall usability of the GMSL Link Margin testing tool.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.04.1
Release Date: 2026-4-22
Added
- GMSL Margin Test: Added support for testing GMSL connection quality, allowing users to evaluate signal integrity and link reliability.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.03.1
Release Date: 2026-3-30
Added
- Recondition Tool: Added support for recovering devices with broken or corrupted firmware, going beyond standard firmware update functionality.
Changed
- Simulation Improvements: Optimized layout of Simulation 4.
- Simulation Improvements: Added config section caching for same-device cameras — profile selection now carries over automatically when switching between cameras of the same device.
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v26.01.1
Release Date: 2026-1-30
Added
- Profile Management: Added support for saving OSP profiles as system profiles and system profiles as OSP profiles
- IMU preivew feature: Added IMU preview feature with live data streaming support
Changed
- Simulation Improvements: Resolved restriction that prevented simultaneous camera selection in main page and simulation page. Users can now select cameras in both views concurrently
- Software Zoom Removed: Removed software zoom feature to maintain single source of truth through hardware ISP control only
- File Picker: Add file picker to windows platform
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v25.12.1
Release Date: 2025-12-8
Added
- Platform Support: Added support for Raspberry Pi 4 and 5.
- ISP Controls: Added eHDR support to control mode.
- Device Configuration: Added route config settings(.yaml) for IMX93 and IMX95.
- Firmware update: Now automatically falls back to offline mode using local resources if online resources have issues
Changed
- Simulation: Removed individual streaming buttons to streamline the interface.
- Responsive layout improvement: The layout now automatically switches back to 3 columns when the window is resized larger
- Easier drag control: Increased the dropzone size for dragging the control section
Fixed
- Fixed various minor bugs and improved overall stability.
Download
v25.10.1
Release Date: 2025-10-21
Added
- ISP controls: Added special effects and flicker mode options to control mode
- ISP ROI control: Added region of interest controls to control mode
- Preivew: Added zoom and grid overlay features to the preview section
- Simulation: Added buttons to start/stop streaming for all cameras simultaneously
Fixed
- Fixed various minor bugs and improved overall stability
Download
v25.09.1
Release Date: 2025-9-25
Added
- Logging System: Implemented a new system. Users can now export log files for improved troubleshooting.
- Image Save Options: Users can now save images in BMP, PNG, JPG formats, or direct buffer.
- Recording: Added a new recording feature with support for FFV1 and OpenH264 codecs.
- Preferred Stream Format: Users can now select prefered stream format in options.
Fixed
- Addressed various minor bugs and improved overall stability.
Download
v25.08.2
Release Date: 2025-08-30
Added
- Draggable layout functionality for customizable workspace
- Color theme selection feature
- Custom logo functionality
Changed
- Completely redesigned user interface with modern design
- Streamlined interface by focusing on core functionality
Download
v25.06.1
Release Date: 2025-06-30
Changed
- Added support for more camera module firmware updates
- Fixed timeout issue when starting streaming at high resolution on i.MX8MM
Download
v25.04.1
Release Date: 2025-04-10
Added
- Integration with VizionSDK Vx API
- Focus Mode
- Exposure Range adjustment in Exposure Auto Mode
- Capture Info displaying current Timestamp and FrameCount
Improved
- Real-time progress feedback during firmware update
Download
v25.03.1
Release Date: 2025-03-18
Added
- FPS display in streaming window
- Improved stability of TEVS firmware updates
Fixed
- Jetson platform streaming issue
- Jetson Orin EVK TEVS Camera firmware update issue
- i.MX8MM streaming issue with large resolutions
Download
- NVIDIA JetPack 5.x, JetPack 6.x: Download
v24.11.1
Release Date: 2024-11-13
Added
- Support for UP Squared Pro 7000 platform
- Support for NVIDIA JetPack 6.x platform
Fixed
- i.MX8MM unable to list MIPI Camera
- TEVS camera streaming issue after firmware upgrade
Download
- Linux (Debian) x64: Download (Compatible with UP Squared Pro 7000)
- NXP-iMX (iMX8MP, iMX8MM, iMX93): Download
- NVIDIA JetPack 5.x: Download
- TI TDA4VM: Download
v24.08.3
Release Date: 2024-08-20
Added
- AGC mode in exposure settings
- NV12 in preferred format settings
- VizionCTL in Windows package
Fixed
- Non-UVC camera opening issue
- UVC updater loading speed
- Software update button unclickable after license activation
Download
- Windows 10/11 x64: Download
- Linux (Debian) x64: Download
- NXP-iMX (iMX8MP, iMX8MM, iMX93): Download
- NVIDIA JetPack 5.x: Download
- TI TDA4VM: Download
v24.06.1
Release Date: 2024-06-06
Added
- Preferred format setting
- NXP iMX93 support
- Option to disable networking requests on Windows
Changed
- Exposure max value set to 1000000
Fixed
- Exposure max value textbox length
- Pop-up window size issue
Download
- Windows 10/11 x64: Download
- Linux (Debian) x64: Download
- NXP-iMX (iMX8MP, iMX8MM, iMX93): Download
- NVIDIA JetPack 5.x: Download
v24.03.2
Release Date: 2024-03-11
Added
- Stable version for JetPack 4
Fixed
- Video and image path editing
- FPS decimal point display
Download
- Windows 10/11 x64: Download
- Linux (Debian) x64: Download
- NXP-iMX (iMX8MP, iMX8MM): Download
- NVIDIA JetPack 5.x: Download
- NVIDIA JetPack 4.x: Download
v24.03.1
Release Date: 2024-03-05
Fixed
- Application update not working on Windows
- Crash dialog on Linux
- USB2.0 ISP firmware update issue
Download
v24.02.1
Release Date: 2024-02-05
Added
- OSP (On Sensor Profile) feature
- Firmware update management
- Multiple camera simulation
- UID in device list selection
Changed
- Disabled automatic camera activation on startup
- Disabled automatic OS profile activation when opening camera