Log File Setting
Introduction
These functions are responsible for setting the log from a camera.
HelloVizionSDK
Function:
- C++
- Python
- C#
- C
void HelloVizionSDK()
def HelloVizionSDK()
void HelloVizionSDK()
void hello_vizionsdk()
Function Description:
- This function is used to get the version of the VizionSDK from the log.
Parameter Description:
- This function does not take any input parameters.
Example:
- C++
- Python
- C#
- C
HelloVizionSDK();
// Hello VizionSDK!
// Version: {VizionSDK Version}
pyvizionsdk.HelloVizionSDK()
# Hello VizionSDK!
# Version: {VizionSDK Version}
CSVizionSDK.HelloVizionSDK();
// Hello VizionSDK!
// Version: {VizionSDK Version}
hello_vizionsdk();
// Hello VizionSDK!
// Version: {VizionSDK Version}
VxSetLogFile
Function:
- C++
- Python
- C#
- C
int VxSetLogFile(const std::string& folderPath)
def VxSetLogFile(folderPath)
int VxSetLogFile(string folderPath)
int vx_set_log_file(const char* folderPath)
Function Description:
- This function is used to set the destination path where to save the log file.
Parameter Description:
-
folderPath : A string constants of folder path.
-
Return : return 0 = PASS, return -1 = FAIL.
Example:
- C++
- Python
- C#
- C
const std::string folderPath = "LOG_PATH";
// set the destination path of log file
VxSetLogFile(folderPath);
folderPath = "LOG_PATH"
# set the destination path of log file
pyvizionsdk.VxSetLogFile(folderPath)
string folderPath = "LOG_PATH";
// set the destination path of log file
CSVizionSDK.VxSetLogFile(folderPath);
const char* folderPath = "LOG_PATH";
// set the destination path of log file
vx_set_log_file(folderPath);
VxSetLogLevel
Function:
- C++
- Python
- C#
- C
void VxSetLogLevel(VX_LOG_LEVEL level)
def VxSetLogLevel(level)
void VxSetLogLevel(VX_LOG_LEVEL level)
void vx_set_log_level(vx_log_level level)
Function Description:
- This function is for setting the log level, determining the verbosity of log messages.
Parameter Description:
-
level : The parameter is a VX_LOG_LEVEL variable that represents the level of the log.
infoLogging levels follow an order from low to high, meaning that setting a specific level enables logging for that level and all higher severity levels.
-
VX_LOG_LEVEL format:
- C++
- Python
- C#
- C
// Ordered from Low to High
enum class VX_LOG_LEVEL {
VX_LOG_LEVEL_TRACE,
VX_LOG_LEVEL_DEBUG,
VX_LOG_LEVEL_INFO,
VX_LOG_LEVEL_WARN,
VX_LOG_LEVEL_ERROR,
VX_LOG_LEVEL_CRITICAL,
VX_LOG_LEVEL_OFF,
}# Ordered from Low to High
class VX_LOG_LEVEL(Enum):
VX_LOG_LEVEL_TRACE = 0
VX_LOG_LEVEL_DEBUG = 1
VX_LOG_LEVEL_INFO = 2
VX_LOG_LEVEL_WARN = 3
VX_LOG_LEVEL_ERROR = 4
VX_LOG_LEVEL_CRITICAL = 5
VX_LOG_LEVEL_OFF = 6// Ordered from Low to High
public enum VX_LOG_LEVEL {
VX_LOG_LEVEL_TRACE,
VX_LOG_LEVEL_DEBUG,
VX_LOG_LEVEL_INFO,
VX_LOG_LEVEL_WARN,
VX_LOG_LEVEL_ERROR,
VX_LOG_LEVEL_CRITICAL,
VX_LOG_LEVEL_OFF,
}// Ordered from Low to High
typedef enum vx_log_level {
VX_LOG_LEVEL_TRACE = 0,
VX_LOG_LEVEL_DEBUG = 1,
VX_LOG_LEVEL_INFO = 2,
VX_LOG_LEVEL_WARN = 3,
VX_LOG_LEVEL_ERROR = 4,
VX_LOG_LEVEL_CRITICAL = 5,
VX_LOG_LEVEL_OFF = 6,
} vx_log_level;
Example:
- C++
- Python
- C#
- C
// Set the log level to information level
VxSetLogLevel(VX_LOG_LEVEL::VX_LOG_LEVEL_INFO);
from pyvizionsdk import VX_LOG_LEVEL
# Set the log level to information level
pyvinzionsdk.VxSetLogLevel(VX_LOG_LEVEL.VX_LOG_LEVEL_INFO)
// Set the log level to information level
CSVizionSDK.VxSetLogLevel(VX_LOG_LEVEL.VX_LOG_LEVEL_INFO);
// Set the log level to information level
vx_set_log_level(VX_LOG_LEVEL_INFO);
Explanation of Levels(Ordered from Low to High):
VX_LOG_LEVEL_TRACE: Provides the most detailed logging, capturing step-by-step execution flow.VX_LOG_LEVEL_DEBUG: Includes debugging information for developers, offering insights into internal operations and variable states.VX_LOG_LEVEL_INFO(Default) : Logs general operational events, such as initialization, configuration changes, and so on.VX_LOG_LEVEL_WARN: Highlights potential issues that do not immediately impact functionality.VX_LOG_LEVEL_ERROR: Captures critical issues that disrupt specific functionalities but do not cause system-wide failure.VX_LOG_LEVEL_CRITICAL: Logs severe errors that may lead to system or application failure, requiring urgent attention.VX_LOG_LEVEL_OFF: Disables all logging, preventing any messages from being recorded.
VxSetLogCallback
Function:
- C++
- C
void VxSetLogCallback(VxLogCallback callback, void* userData)
void vx_set_log_callback(vx_log_callback callback, void* userData)
Function Description:
- This function registers a callback to receive SDK log messages. Once set, the callback is invoked for every log message at or above the current log level.
Parameter Description:
-
callback : A function pointer matching the
VxLogCallbacksignature:- C++
- C
using VxLogCallback = void (*)(VX_LOG_LEVEL level, const char* message, void* userData);typedef void (*vx_log_callback)(vx_log_level level, const char* message, void* userData); -
userData : An arbitrary pointer passed back unchanged to the callback on every invocation. Pass
NULL/nullptrif not needed. -
Return : This function does not return a value.
Example:
- C++
- C
void MyLogHandler(VX_LOG_LEVEL level, const char* message, void* userData) {
std::cout << "[SDK] " << message << std::endl;
}
// Register the log callback
VxSetLogCallback(MyLogHandler, nullptr);
void my_log_handler(vx_log_level level, const char* message, void* userData) {
printf("[SDK] %s\n", message);
}
/* Register the log callback */
vx_set_log_callback(my_log_handler, NULL);
VxClearLogCallback
Function:
- C++
- C
void VxClearLogCallback()
void vx_clear_log_callback()
Function Description:
- This function unregisters the currently active log callback. After this call, SDK log messages are no longer forwarded to the previously registered callback.
Parameter Description:
-
This function does not take any input parameters.
-
Return : This function does not return a value.
Example:
- C++
- C
// Unregister the log callback
VxClearLogCallback();
/* Unregister the log callback */
vx_clear_log_callback();