Building an Image in Docker Container
Introduction
Set up the build environment using container methods.
Set up build environment on host PC:
The build environment is tested under Ubuntu 22.04.
Install required package:
sudo apt install docker.io
Download TechNexion's dockerfile:
wget https://raw.githubusercontent.com/TechNexion/meta-tn-imx-bsp/kirkstone_5.15.71-2.2.0-stable/tools/container/dockerfile
Build the docker container:
sudo docker build -t tn-develop-ubuntu .
Check the built docker container:
$ sudo docker images
REPOSITORY TAG IMAGE ID CREATED SIZE
tn-develop-ubuntu latest b438b5e2e8fb 5 minutes ago 2.15GB
ubuntu 20.04 88bd68917189 8 weeks ago 72.8MB
Use docker container:
Use this docker container to start building Yocto image.
Create a new docker container:
$ sudo docker run -it -u jenkins -v ${directory_in_host_machine}:${directory_in_docker} tn-develop-ubuntu bash
(-v: use to bind volume to the directory in host machine to a directory in docker)
(password: jenkins)
To run a command as administrator (user "root"), use "sudo <command>".
See "man sudo_root" for details.
jenkins@818cacdead74:/$ cd
jenkins@818cacdead74:~$
info
On Ubuntu 22 container the seccomp protection feature of docker has to be disabled when creating the build container by adding the parameter --security-opt seccomp=unconfined after the -it parameter in the command line above.
Re-entry is required when exiting:
$ sudo docker start <your container id>
$ sudo docker attach <your container id>
e.g.
$ sudo docker ps -a
CONTAINER ID IMAGE COMMAND CREATED STATUS PORTS NAMES
818cacdead74 tn-develop-ubuntu "bash" 45 minutes ago Exited (0) 19 seconds ago hopeful_villanir
$ sudo docker start 818cacdead74
$ sudo docker attach 818cacdead74