Testing Wireless LAN (WiFi)
Test Wireless LAN in Station (STA) mode
In station mode, unit establishes a connection to a nearby access point. This is normally abbreviated as "STA" mode. The other mode is Access Point mode (or "AP" mode). AP mode is covered further down in this article.
WIFI connection
Check if the wifi module is loaded.
For QCA WLAN:
~# lsmod
Module Size Used by
wlan 4673536 0
Run "connmanctl" in interactive mode.
~# connmanctl
Scan and list the wifi hotspots, then register the agent to handle user requests.
connmanctl> scan wifi
Scan completed for wifi
connmanctl> services
hotspot wifi_4439c4970d84_544543484e4558494f4e_managed_psk
connmanctl> agent on
Agent registered
Connect to the hotspot and enter the passphrase.
connmanctl> connect wifi_4439c4970d84_544543484e4558494f4e_managed_psk
Agent RequestInput wifi_4439c4970d84_544543484e4558494f4e_managed_psk
Passphrase = [ Type=psk, Requirement=mandatory, Alternates=[ WPS ] ]
WPS = [ Type=wpspin, Requirement=alternate ]
Passphrase?
Connected wifi_4439c4970d84_544543484e4558494f4e_managed_psk
Quit the interactive mode of "connmanctl":
connmanctl> quit
Test if wifi actually works.
~# ping www.google.com
PING www.google.com (203.66.124.251): 56 data bytes
64 bytes from 203.66.124.251: seq=0 ttl=59 time=4.905 ms
64 bytes from 203.66.124.251: seq=1 ttl=59 time=12.278 ms
64 bytes from 203.66.124.251: seq=2 ttl=59 time=4.307 ms
For the next boot, connman will automatically connect to the hotspot you used before.
Test WIFI Access Point (AP) mode
In this tutorial, the unit is connected via physical Ethernet port to a local network.
In our default builds in Yocto when you connect an Ethernet cable to the unit, the unit will attempt to establish a network connection to the local network, including getting an IP address from the local DHCP server. If for some reason this doesn't occur, you can start a DHCP client yourself to get an IP address:
~# udhcpc -i eth0
udhcpc: started, v1.27.2
udhcpc: sending discover
udhcpc: sending select for 10.20.30.157
udhcpc: lease of 10.20.30.157 obtained, lease time 1200
/etc/udhcpc.d/50default: Adding DNS 10.20.30.240
/etc/udhcpc.d/50default: Adding DNS 1.1.1.1
/etc/udhcpc.d/50default: Adding DNS 168.95.192.1
Create hotspot with WPA + WPA2 passphrase.
~# connmanctl tether wifi on <ssid> <passphrase>
e.g.
~# connmanctl tether wifi on SAP 12345678
Use another device such as a mobile phone to connect to the access point SAP to get wifi connectivity.
Unlike a station connection to an Access Point, tether interfaces are not persistent across reboots.
Clean the stored settings of hotspot.
~# rm /var/lib/connman/*/settings
Switch off wifi
~# connmanctl disable wifi
Switch on wifi
~# connmanctl enable wifi
Operating WIFI in Concurrent Mode
In many situations there may not be a wired connection available. TechNexion wireless modules such as the QCA9377 can operate in concurrent mode. In concurrent mode, it can be treated as an access point and can also establish a connection to a local access point as a Station, and then bridge the two connections. One example where you might find this useful in when provisioning a device into a wireless network for the first time.
If when you boot your unit and after running ifconfig you do not see a p2p0 interface, the QCA9377 kernel driver (loadable module) has not been built to enable the P2P node, so this much be turned to enable concurrent mode for NAT/forwarding usage by re-compiling wifi module. By default, distributions built with Yocto Project enable the P2P interface.
CONFIG_P2P_INTERFACE=y
For more detail information for building the wifi module, please refer to the following link: https://github.com/TechNexion/qcacld-2.0
Check that all of the required interfaces are present
After enabling the P2P node of wifi driver and boot up the system to check the P2P0 node is exist or not?To check the mainly two nodes p2p0 and wlan0
root@xore-imx8mm:~# ifconfig -a
eth0 Link encap:Ethernet HWaddr a6:4a:23:a5:03:f4
UP BROADCAST MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:2 errors:0 dropped:0 overruns:0 frame:0
TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:140 (140.0 B) TX bytes:140 (140.0 B)
p2p0 Link encap:Ethernet HWaddr 02:1f:7b:b5:8f:f6
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:3000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
wlan0 Link encap:Ethernet HWaddr 00:1f:7b:31:8f:f6
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:3000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
To ensure all of wireless network setting has been cleared.
root@xore-imx8mm:~# rm -rf /var/lib/connman/
The Yocto system was using CONNMAN utility for networking management in default and executed the connmanctl utility in the command line:
root@xore-imx8mm:~# connmanctl
Setup the tethering peer and make the p2p0 port enter forwarding state
connmanctl> tether wifi myAP 12345678
Wifi SSID set
Wifi passphrase set
where: SSID = myAP; passphrase = 12345678
connmanctl> tether wifi on
connmanctl> [ 369.346704] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
Enabled tethering for wifi
connmanctl> [ 369.669782] tether: port 1(p2p0) entered blocking state
[ 369.675374] tether: port 1(p2p0) entered disabled state
[ 369.680937] device p2p0 entered promiscuous mode
[ 369.685632] audit: type=1700 audit(1588753496.488:4): dev=p2p0 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
[ 369.686241] IPv6: ADDRCONF(NETDEV_CHANGE): p2p0: link becomes ready
[ 369.697038] audit: type=1300 audit(1588753496.488:4): arch=c00000b7 syscall=29 success=yes exit=0 a0=14 a1=89a2 a2=fffffad79818 a3=ffffffffffffffff items=0 ppid=1 pid=2804 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="connmand" exe="/usr/sbin/connmand" key=(null)
[ 369.704286] tether: port 1(p2p0) entered blocking state
[ 369.731672] audit: type=1327 audit(1588753496.488:4): proctitle=2F7573722F7362696E2F636F6E6E6D616E64002D6E
[ 369.736871] tether: port 1(p2p0) entered forwarding state
Connecting the wifi to another access point
Adapt the wireless antenna and start to do scan the useful access point in the near field:
connmanctl> scan wifi
Scan completed for wifi
List the services to show the access points available:
connmanctl> services
TECHNEXION-RDTEST wifi_021f7bb58ff6_544543484e4558494f4e2d524454455354_managed_psk
TECHNEXION-RDTEST wifi_001f7b318ff6_544543484e4558494f4e2d524454455354_managed_psk
Select the service id based on the physical MAC address of wlan0 node:
When the P2P interface is enabled, for every access point service available (physically), you will see two services listed. One of them includes the physical MAC address of the wlan0 interface (always starts with wifi_001f7b... in TechNexion products). The other is a slightly modified virtual service belonging to the p2p0 interface (usually starts with wifi_021f7b). When tethering, you need to connect to the service with the physical MAC address of wlan0.
connmanctl> agent on
Agent registered
connmanctl> connect wifi_001f7b318ff6_544543484e4558494f4e2d524454455354_managed_psk
Agent RequestInput wifi_001f7b318ff6_544543484e4558494f4e2d524454455354_managed_psk
Passphrase = [ Type=psk, Requirement=mandatory, Alternates=[ WPS ] ]
WPS = [ Type=wpspin, Requirement=alternate ]
Passphrase? <Enter access point password here>
onnmanctl> [ 1619.839276] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[ 1630.578209] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1630.589920] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 1630.606166] audit: type=1325 audit(1588754757.424:6): table=nat family=2 entries=0
[ 1630.684170] audit: type=1300 audit(1588754757.424:6): arch=c00000b7 syscall=273 success=yes exit=0 a0=a a1=419fd0 a2=0 a3=aitems=0 ppid=2804 pid=2908 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295comm="modprobe" exe="/bin/kmod" key=(null)
[ 1630.709978] audit: type=1327 audit(1588754757.424:6): proctitle=2F7362696E2F6D6F6470726F62650069707461626C655F6E6174002D71
[ 1630.872002] audit: type=1325 audit(1588754757.512:7): table=nat family=2 entries=5
[ 1630.879669] audit: type=1300 audit(1588754757.512:7): arch=c00000b7 syscall=208 success=yes exit=0 a0=1b a1=0 a2=40 a3=1f02ea00items=0 ppid=1 pid=2804 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295comm="connmand" exe="/usr/sbin/connmand" key=(null)
[ 1630.906405] audit: type=1327 audit(1588754757.512:7): proctitle=2F7573722F7362696E2F636F6E6E6D616E64002D6E
connmanctl> quit
After leaving the connection manager, we could check there is a tether peer was added and assigned a IP address of class c network segment.
root@xore-imx8mm:~# ifconfig
eth0 Link encap:Ethernet HWaddr a6:4a:23:a5:03:f4
UP BROADCAST MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:6882 errors:0 dropped:0 overruns:0 frame:0
TX packets:6882 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:495500 (483.8 KiB) TX bytes:495500 (483.8 KiB)
p2p0 Link encap:Ethernet HWaddr 02:1f:7b:b5:8f:f6
inet6 addr: fe80::1f:7bff:feb5:8ff6/64 Scope:Link
UP BROADCAST RUNNING MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:64 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:3000
RX bytes:0 (0.0 B) TX bytes:11196 (10.9 KiB)
tether Link encap:Ethernet HWaddr 02:1f:7b:b5:8f:f6
inet addr:192.168.0.1 Bcast:192.168.0.255 Mask:255.255.255.0
inet6 addr: fe80::e02d:e4ff:fed6:dbb7/64 Scope:Link
UP BROADCAST RUNNING MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:44 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:7855 (7.6 KiB)
wlan0 Link encap:Ethernet HWaddr 00:1f:7b:31:8f:f6
inet addr:xx.xx.xx.99 Bcast:10.88.88.255 Mask:255.255.255.0
inet6 addr: fe80::21f:7bff:fe31:8ff6/64 Scope:Link
UP BROADCAST RUNNING MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:100 errors:0 dropped:0 overruns:0 frame:0
TX packets:53 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:3000
RX bytes:12613 (12.3 KiB) TX bytes:10497 (10.2 KiB)
Now the wifi concurrent mode setup is complete.
Connecting and testing concurrent mode
There are so many ways to find or scan the SSID of access point that we just set earlier (e.g. PC or cell phone). You can use your cell phone to connect to the hotspot (myAP) as usual and start using the Internet or networking.
Troubleshooting
- Duplicated AP name shows when scanning wifi hotspots:
e.g.
connmanctl> services
TECHNEXION(5G) wifi_001f7b311132_544543484e4558494f4e28354729_managed_psk
TECHNEXION(5G) wifi_021f7bb51132_544543484e4558494f4e28354729_managed_psk
The string:
wifi_001f7b311132_544543484e4558494f4e28354729_managed_psk
The prefix 001f7b is the MAC address specifically for TechNexion WIFI chip.
wifi_021f7bb51132_544543484e4558494f4e28354729_managed_psk
The prefix 021f7b is the virtual MAC address generated for p2p interface. (Note: This virtual MAC address follows the administered addresses rule to be generated.)
If you don't want p2p to show in hotspot scan: iw dev p2p0 del