Controlling Backlight
If there is an LCD present and connected to the system, the backlight brightness can be controlled by reading and writing to files in the /sys filesystem (sysfs).
# cd /sys/class/backlight/backlight
# cat max_brightness
100
The max_brightnessfile contains a value that pertains to the maximum brightness of the backlight. The brightness level can be controlled by writing a number between 0 and max_brightnessto the brightnessfile.
# cat brightness
50
Off:
# echo 0 > brightness
50%:
# echo 50 > brightness
Maximum:
# echo 100 > brightness