Skip to main content

Camera Control

Introduction

These functions are responsible for controlling various parameters of the camera.

VxResetUVC

Function:

int VxResetUVC(std::shared_ptr<VxCamera> vxcam)

Function Description:

  • This function is for resetting the UVC device.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • return 0 = PASS, return -1 = FAIL.

Example:

// reset the UVC device
VxResetUVC(vxcam);

VxGetUVCImageProcessingRange

Function:

int VxGetUVCImageProcessingRange(std::shared_ptr<VxCamera> vxcam,
VX_UVC_IMAGE_PROPERTIES propId,
long& min,
long& max,
long& step,
long& def)

Function Description:

  • This function is for the UVC device to get the range of image processing parameters.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_UVC_IMAGE_PROPERTIES format UVC image processing property for which the range is being queried.
  • min : A long type variable to store the minimum allowable value for the property.
  • max : A long type variable to store the maximum allowable value for the property.
  • step : A long type variable to store the step value for the property.
  • def : A long type variable to store the default value for the property.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, min, max, step, def)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

long min = 0, max = 0, step = 0, def = 0;
auto propId = static_cast<VX_UVC_IMAGE_PROPERTIES>(0);
// get the UVC image processing range
VxGetUVCImageProcessingRange(vxcam, propId, min, max, step, def);

VxGetUVCImageProcessing

Function:

int VxGetUVCImageProcessing(std::shared_ptr<VxCamera> vxcam,
VX_UVC_IMAGE_PROPERTIES propId,
long& value,
int& flag)

Function Description:

  • This function is for the UVC device to get the image processing parameters’ current value and the flag to indicate whether the property is in auto mode or not.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_UVC_IMAGE_PROPERTIES format UVC image processing property for which being queried.
  • value : A long type variable to store the current value of the property.
  • flag : An int type variable to indicate whether the property is read only or not. If the flag is 1, it means the property is in auto mode for read-only.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, value, flag)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

long value = 0;
int flag = 0;
auto propId = static_cast<VX_UVC_IMAGE_PROPERTIES>(0);
// get the UVC image processing
VxGetUVCImageProcessing(vxcam, propId, value, flag);

VxSetUVCImageProcessing

Function:

int VxSetUVCImageProcessing(std::shared_ptr<VxCamera> vxcam,
VX_UVC_IMAGE_PROPERTIES propId,
long value,
int flag)

Function Description:

  • This function is for the UVC device to set image processing parameters value and the flag.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_UVC_IMAGE_PROPERTIES format UVC image processing property for which being queried.
  • value : A long type variable to set the value of the property.
  • flag : A int type variable to indicate whether the property is read only or not. If the flag is 1, it means the property is in auto mode for read-only.
  • return 0 = PASS, return -1 = FAIL.

Example:

// set the brightness to 16
VxSetUVCImageProcessing(vxcam, VX_UVC_IMAGE_PROPERTIES::UVC_IMAGE_BRIGHTNESS, 16, 0);

VxGetISPImageProcessingRange

Function:

int VxGetISPImageProcessingRange(std::shared_ptr<VxCamera> vxcam,
VX_ISP_IMAGE_PROPERTIES propId,
int& min,
int& max,
int& step,
int& def)

Function Description:

  • This function is for the ISP device to get the range of image processing parameters.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_ISP_IMAGE_PROPERTIES format ISP image processing property for which the range is being queried.
  • min : An integer type variable to store the minimum allowable value for the property.
  • max : An integer type variable to store the maximum allowable value for the property.
  • step : An integer type variable to store the step value for the property.
  • def : An integer type variable to store the default value for the property.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, min, max, step, def)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

int min = 0, max = 0, step = 0, def = 0;
auto propId = static_cast<VX_ISP_IMAGE_PROPERTIES>(0);
// get the ISP image processing range
VxGetISPImageProcessingRange(vxcam, propId, min, max, step, def);

VxGetISPImageProcessing

Function:

int VxGetISPImageProcessing(std::shared_ptr<VxCamera> vxcam,
VX_ISP_IMAGE_PROPERTIES propId,
int& value,
int& flag)

Function Description:

  • This function is for the ISP device to get an image processing parameter value and the flag.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_ISP_IMAGE_PROPERTIES format ISP image processing property for which being queried.
  • value : An integer type variable to store the current value of the property.
  • flag : An integer type variable to indicate whether the property is read only or not. If the flag is 1, it means the property is read-only.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, value, flag)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

int value;
int flag = 0;
// get the ISP image processing value and flag
VxGetISPImageProcessing(vxcam, VX_ISP_IMAGE_PROPERTIES::ISP_IMAGE_BRIGHTNESS, value, flag);

VxSetISPImageProcessing

Function:

int VxSetISPImageProcessing(std::shared_ptr<VxCamera> vxcam,
VX_ISP_IMAGE_PROPERTIES propId,
int value)

Function Description:

  • This function is for the ISP device to set an image processing parameter value.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • propId : A VX_ISP_IMAGE_PROPERTIES format ISP image processing property for which being queried.
  • value : An integer type variable to set the value of the property.
  • return 0 = PASS, return -1 = FAIL.

Example:

// set the brightness to 16
VxSetISPImageProcessing(vxcam, VX_ISP_IMAGE_PROPERTIES::ISP_IMAGE_BRIGHTNESS, 16);

VxSetISPImageProcessingDefault

Function:

int VxSetISPImageProcessingDefault(std::shared_ptr<VxCamera> vxcam)

Function Description:

  • This function is for the ISP device to set an image processing parameter to the default value.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • return 0 = PASS, return -1 = FAIL.

Example:

// set the ISP image processing to default value
VxSetISPImageProcessingDefault(vxcam);

VxGetCurrentGain

Function:

int VxGetCurrentGain(std::shared_ptr<VxCamera> vxcam, uint8_t& gain)

Function Description:

  • This function is for the device to obtain the current exposure gain value.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • gain : A reference of the uint8_t(byte) variable that stores the gain value.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, gain)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

uint8_t gain;
// get the gain value
VxGetCurrentGain(vxcam, gain);

VxGetCurrentExposure

Function:

int VxGetCurrentExposure(std::shared_ptr<VxCamera> vxcam, uint32_t& exp)

Function Description:

  • This function is for the device to obtain the current exposure time value.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • exp : A reference of the uint32_t(uint) variable which stored the exposure value.
  • Return:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : tuple(return_code, exp)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

uint32_t exp;
// get the exposure time value
VxGetCurrentGain(vxcam, exp);

VxGetMaxFPS & VxSetMaxFPS

Function:

int VxGetMaxFPS(std::shared_ptr<VxCamera> vxcam, uint8_t& fps)
int VxSetMaxFPS(std::shared_ptr<VxCamera> vxcam, uint8_t fps)

Function Description:

  • VxGetMaxFPS : This function is for retrieving the maximum frame rate supported by the camera.
  • VxSetMaxFPS : This function is for the device to set the maximum frame rate

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • fps : A reference of a uint8_t(byte) variable that will be used to get or set the maximum frame rate.
  • VxGetMaxFPS :
    • C++ / C# : return 0 = PASS, return -1 = FAIL

    • Python : return tuple(return_code, fps)

      return_code: return 0 = PASS, return -1 = FAIL

    • VxSetMaxFPS : return 0 = PASS, return -1 = FAIL.

Example:

uint8_t max_fps;
// get the maximum frame rate
VxGetMaxFPS(vxcam, max_fps);
// Set the frame rate to the maximum value
VxSetMaxFPS(vxcam, max_fps);

VxGetThroughPut & VxSetThroughPut

Function:

int VxGetThroughPut(std::shared_ptr<VxCamera> vxcam, uint16_t& throughPut)
int VxSetThroughPut(std::shared_ptr<VxCamera> vxcam, uint16_t throughPut)

Function Description:

  • VxGetThroughPut : This function is for retrieving the throughput value from the camera.
  • VxSetThroughPut : This function is for the device to set the throughput value.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().

  • throughPut : A uint16_t(ushort) variable that will be used to get or set the throughput value.

  • VxGetThroughPut :

    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python : return tuple(return_code, throughPut)

      return_code : return 0 = PASS, return -1 = FAIL

  • VxSetThroughPut : return 0 = PASS, return -1 = FAIL.

Example:

uint16_t throughPut;
// get the throughPut
VxGetThroughPut(vxcam, throughPut);
// set the throughPut
VxSetThroughPut(vxcam, throughPut);

VxGetTimestamp & VxGetFrameCount

Function:

int VxGetTimestamp(std::shared_ptr<VxCamera> vxcam, float& timestamp)
int VxGetFrameCount(std::shared_ptr<VxCamera> vxcam, uint8_t& frameCount)

Function Description:

  • VxGetTimeStamp : This function is for retrieving the timestamp value from the camera.
  • VxGetFrameCount : This function is for retrieving the frame count value from the camera.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • timestamp : A float variable that will be used to get the timestamp value.
  • frameCount : A uint8_t(byte) variable that will be used to get the frame count value.
  • VxGetTimestamp & VxGetFrameCount:
    • C++ / C# : return 0 = PASS, return -1 = FAIL
    • Python :
      1. VxGetTimestamp : return tuple(return_code, timestamp)
      2. VxGetFrameCount : return tuple(return_code, frameCount)

      return_code : return 0 = PASS, return -1 = FAIL

Example:

// get image
uint8_t* raw_data = new uint8_t[3840 * 2160 * 2];
int raw_size = 0;
VxGetImage(vxcam, raw_data, &raw_size, 3000)

// get the timestamp and frame count value after getting image
float timestamp;
uint8_t framecnt;
VxGetTimestamp(vxcam, timestamp);
VxGetFrameCount(vxcam, framecnt);
std::cout << "TimeStamp: " << timestamp << std::endl;
std::cout << "framecnt: " << framecnt << std::endl;

VxResetTimestamp & VxResetFrameCount

warning

These reset functions must be used when the camera is not in standby mode.

Function:

int VxResetTimestamp(std::shared_ptr<VxCamera> vxcam)
int VxResetFrameCount(std::shared_ptr<VxCamera> vxcam)

Function Description:

  • VxResetTimeStamp : This function is for resetting the timestamp value from the camera.
  • VxResetFrameCount : This function is for resetting the frame count value from the camera.

Parameter Description:

  • vxcam : A pointer shared ownership of a camera obtained from VxInitialCameraDevice().
  • VxResetTimestamp & VxResetFrameCount: return 0 = PASS, return -1 = FAIL

Example:

// start streaming
VxStartStreaming(vxcam);
// reset the timestamp and frame count
VxResetTimestamp(vxcam);
VxResetFrameCount(vxcam);

Parameter Structure

VX_UVC_IMAGE_PROPERTIES

enum class VX_UVC_IMAGE_PROPERTIES {
UVC_IMAGE_BRIGHTNESS,
UVC_IMAGE_CONTRAST,
UVC_IMAGE_HUE,
UVC_IMAGE_SATURATION,
UVC_IMAGE_SHARPNESS,
UVC_IMAGE_GAMMA,
UVC_IMAGE_COLORENABLE,
UVC_IMAGE_WHITEBALANCE,
UVC_IMAGE_BACKLIGHT_COMPENSATION,
UVC_IMAGE_GAIN,
UVC_IMAGE_PAN,
UVC_IMAGE_TILT,
UVC_IMAGE_ROLL,
UVC_IMAGE_ZOOM,
UVC_IMAGE_EXPOSURE,
UVC_IMAGE_IRIS,
UVC_IMAGE_FOCUS,
UVC_IMAGE_PROP_MAX
}

VX_ISP_IMAGE_PROPERTIES

ISP Image PropertiesminmaxstepdefaultDescriptionNotes
BRIGHTNESS-101010
CONTRAST-505010
SATURATION050110
WHITEBALANCE_MODE0111Manual Temperature (0)
Auto (1)
WHITEBALANCE_TEMPERATURE23001500015000
EXPOSURE_MODE0211Manual Mode (0)
Auto Mode (1)
Auto gain (2)
EXPOSURE_TIME11000000133333
EXPOSURE_MIN_TIME110000001The default value is followed by VxExposure.yaml min value
EXPOSURE_MAX_TIME110000001The default value is followed by VxExposure.yaml max value
EXPOSURE_GAIN16411
GAMMA479122
SHARPNESS-202010
BACKLIGHT_COMPENSATION-150150110
SPECIAL_EFFECT_MODE0410Normal Mode (0)
Black White Mode (1)
Grayscale Mode (2)
Negative Mode (3)
Sketch Mode (4)
DENOISE-202010
FLIP_MODE0310Normal (0)
H-Mirror (1)
V-Mirror (2)
Rotate-180 (3)
PAN01015
TILT01015
ZOOM1080110
FLICK_MODE0310Disable (0)
50Hz (1)
60Hz (2)
Auto (3)
JPEG_QUALITY02551233
TRIGGER_MODE0310Disable (0)
Sync (1)
Periodic (2)
Non Periodic(3)
Supported Device:
  • TEVS cameras
EHDR_MODE0110Enable (0)
Disable (1)
Disable mode will turn off the eHDR effect
EHDR_EXPOSURE_MIN_NUMBER1411
EHDR_EXPOSURE_MAX_NUMBER1414
info

eHDR features are only supported on the following devices:

  • VCS-AR0821 / VCS-AR0822
  • VC-VLS-AR0821 / VC-VLS-AR0822
  • VC-VL-GM2-AR0821 / VC-VL-GM2-AR0822
enum class VX_ISP_IMAGE_PROPERTIES {
ISP_IMAGE_BRIGHTNESS,
ISP_IMAGE_CONTRAST,
ISP_IMAGE_SATURATION,
ISP_IMAGE_WHITEBALANCE_MODE,
ISP_IMAGE_WHITEBALANCE_TEMPERATURE,
ISP_IMAGE_EXPOSURE_MODE,
ISP_IMAGE_EXPOSURE_TIME,
ISP_IMAGE_EXPOSURE_MIN_TIME,
ISP_IMAGE_EXPOSURE_MAX_TIME,
ISP_IMAGE_EXPOSURE_GAIN,
ISP_IMAGE_GAMMA,
ISP_IMAGE_SHARPNESS,
ISP_IMAGE_BACKLIGHT_COMPENSATION,
ISP_IMAGE_SPECIAL_EFFECT_MODE,
ISP_IMAGE_DENOISE,
ISP_IMAGE_FLIP_MODE,
ISP_IMAGE_PAN,
ISP_IMAGE_TILT,
ISP_IMAGE_ZOOM,
ISP_IMAGE_FLICK_MODE,
ISP_IMAGE_JPEG_QUALITY,
ISP_IMAGE_TRIGGER_MODE,
ISP_IMAGE_EHDR_MODE,
ISP_EHDR_EXPOSURE_MIN_NUMBER,
ISP_EHDR_EXPOSURE_MAX_NUMBER,
ISP_IMAGE_PROP_MAX
}