Run Sample
Introduction
This document demonstrates how to use the pyvizionsdk Python SDK with practical examples. You can download the complete sample code from the official repository.
Running the Sample Project
To run the Python sample, open your terminal and execute the following command:
python pyvizionSample.py
Example Usage
Below are some example usages of the pyvizionsdk functions as demonstrated in the sample project.
1. Start the Device
Discover available camera devices and start the device at index 0:
result, camera_list = pyvizionsdk.VxDiscoverCameraDevices()
print("Discovered cameras:", camera_list)
# Print each camera in the list
for camera in camera_list:
print(camera)
# Initialize the camera device at index 0
camera = pyvizionsdk.VxInitialCameraDevice(0)
# Open the camera device
result = pyvizionsdk.VxOpen(camera)
print("Open camera return code:", result)
2. Retrieve Device Information
Get the device name and interface type:
# Get the camera device name
result, name = pyvizionsdk.VxGetDeviceName(camera)
print("Device name:", name)
# Get the interface type name
result, tyname = pyvizionsdk.VxGetDeviceInterfaceType(camera)
print("Device Interface type name:", tyname)
3. Adjust Device Brightness
Retrieve and set the brightness of the device:
# Get UVC image processing brightness
result, brightness, flag = pyvizionsdk.VxGetUVCImageProcessing(camera, VX_UVC_IMAGE_PROPERTIES.UVC_IMAGE_BRIGHTNESS)
print("UVC brightness:", brightness)
print("Flag:", flag)
print("Return code:", result)
# Set the brightness to 12
result = pyvizionsdk.VxSetUVCImageProcessing(camera, VX_UVC_IMAGE_PROPERTIES.UVC_IMAGE_BRIGHTNESS, 12, 0)
print("Set UVC brightness return code:", result)