Configuration & Usage
Configuration Setup
File Locations
After installation, the configuration files will be located at:
- Windows:
C:\Program Files\vizionsdk\bin\VxConfig.conf
C:\Program Files\vizionsdk\bin\VxExposure.yaml - Linux, NXP-iMX, NVIDIA JetPack 6.x and later:
/usr/share/vizionsdk/VxConfig.conf
/usr/share/vizionsdk/VxExposure.yaml
/usr/share/vizionsdk/VxBSLMode.yaml - Local library (Tarball Extraction):
/vizionsdk-{version}-{os}/bin/VxConfig.conf
/vizionsdk-{version}-{os}/bin/VxExposure.yaml
/vizionsdk-{version}-{os}/bin/VxBSLMode.yaml
File Descriptions
- VxConfig: A configuration file used by VizionSDK to recognize TechNexion camera series.
- VxExposure: A YAML file defining the default minimum and maximum exposure time values for each sensor and resolution.
- VxBSLMode: A YAML file defining platform-specific BSL (Bootstrap Loader) profiles for sensor firmware updates on Linux MIPI platforms. Each profile specifies the GPIO hook commands required to enter and exit BSL mode.
You can also customize the location of VxConfig.conf, VxExposure.yaml, and VxBSLMode.yaml by setting the VIZIONSDK_CONFIG_PATH environment variable.
How to use VizionSDK
You can link the VizionSDK library with CMake. For more details, see the Sample Build Guide.
Prerequisites
- CMake (version 3.0 or newer)
- C++ compiler
Import the library
Add the VizionSDK header in your code:
#include "VizionSDK.h"
Build the project with CMake
Using System-Installed SDK (.exe or .deb Installed)
If you installed VizionSDK using the installer, use the following CMake commands:
# Find VizionSDK package
find_package(vizionsdk REQUIRED)
# Link libraries
target_link_libraries(${PROJECT_NAME}
PRIVATE
vizionsdk::VizionSDK
)
Using Extracted SDK Archive
If you are using the SDK directly from the extracted folder, update the paths manually:
# Set path to the SDK library directory
# NOTE: Update this path to match your SDK location
target_include_directories(${PROJECT_NAME}
PRIVATE
<YOUR_SDK_PATH>/include/vizionsdk
)
target_link_directories(${PROJECT_NAME}
PRIVATE
<YOUR_SDK_PATH>/lib
)
# Link libraries
target_link_libraries(${PROJECT_NAME}
PRIVATE
VizionSDK
)
For more detailed information and advanced usage, please refer to the API documentation or the examples on GitHub.