Skip to main content

Forecr Jetson AGX Orin DSBOARD-AGXMAX with JetPack 6.2.2

Instruction​

TechNexion Embedded Vision Solutions provide embedded system developers access to high-performance, industrial-grade camera solutions to accelerate their time to market for embedded vision projects.

Supported Camera Modules​

Camera SeriesProducts
VLS-GM2
VLS-GM2-AR0144
VLS-GM2-AR0145
VLS-GM2-AR0234
VLS-GM2-AR0235
VLS-GM2-AR0246
VLS-GM2-AR0521
VLS-GM2-AR0522
VLS-GM2-AR0544
VLS-GM2-AR0821
VLS-GM2-AR0822
VLS-GM2-AR0830
VLS-GM2-AR1335
VLS-GM2-AR2020
Camera Sensor Comparison

More Camera Products Details...


Supported NVIDIA Jetson Partner Platforms​


Install TN Camera on NVIDIA Jetson Partner Platforms​

Adaptor for NVIDIA Jetson Partner AGX Orin Platforms​

VL-GM2-AGX-8CAM Adaptor for VLS-GM2 Cameras

Connect VL-GM2-AGX-8CAM adaptor to Forecr Jetson AGX Orin DSBOARD-AGXMAX directly.


Follow the video tutorial below to learn how to connect VL-GM2-AGX-8CAM adaptor and VLS-GM2 cameras to DSBOARD-AGXMAX.


Method 1 - Using TechNexion Pre-built modules​

Preparation

We recommend following the installation guide from platform vendors to setup system JetPack 6.2.2. After that, you can follow the below method to install TechNexion Cameras Driver.

  1. Download pre-built modules.

    $ wget https://download.technexion.com/demo_software/EVK/NVIDIA/AGXOrin/pre-built-modules/latest/JP622/tn_camera_modules_jp622.tar.gz
  2. Uncompress the modules.

    $ tar -xf tn_camera_modules_jp622.tar.gz
  3. Run installation script.

    $ cd tn_camera_modules_agx_orin_jp622_<built_time>/
    $ sudo ./tn_install.sh
  4. Run the AGX Orin installer. VLS-GM2 is selected automatically for this package.

    $ sudo ./tn_install.sh
    ****** TechNexion Camera Driver Installation ******
    This installer updates TechNexion camera drivers, camera DTBOs,
    and boot entries for NVIDIA Jetson Development Kits.
    Back up your image before continuing.
    Continue? [Y/n] Y
    Reboot after installation? [y/N] n
    Installing AGX Orin JP62
    Selected module: VLS-GM2
    Installation summary:
    Kernel: 5.15.148-tegra
    Modules installed: 4
    Boot files installed: 5
    Default boot entry: vls-gm2
    Camera overlay: /boot/tegra234-p3737-camera-vls-gm2-overlay.dtbo
    Camera boot entries: 5
    Finish Camera Driver Installation.
    Reboot the device when the user is ready.
tip

You should reboot the device after installation.


Method 2 - Using TechNexion disk image​

info

This disk image file is for VLS-GM2 with Forecr Jetson AGX Orin DSBOARD-AGXMAX with JetPack 6.2.2 version.

  1. Download disk image.

    $ wget https://download.technexion.com/demo_software/EVK/NVIDIA/DSBOARD-AGXMAX/DiskImage/latest/mfi_agx-orin-dsboard-agxmax-gmsl-tn-jp622.tar.gz
  2. Extract the image files.

    $ sudo tar -xf mfi_agx-orin-dsboard-agxmax-gmsl-tn-jp622.tar.gz

    You will see a folder "mfi_jetson-agx-orin-devkit" in your current location.

  3. The platform enters forced recovery mode and connects to the PC via USB.

  4. Write the image files to the platform eMMC.

    $ cd mfi_jetson-agx-orin-devkit
    $ sudo ./tools/kernel_flash/l4t_initrd_flash.sh --flash-only --massflash 1 --network usb0 jetson-agx-orin-devkit --showlogs

Bring up Camera​

TechNexion VizionViewer​

VizionViewer™

Gstreamer​

If you succeed in initialing the camera, you can follow the steps to open the camera.

  1. Check the supported resolutions:

    $ gst-device-monitor-1.0 Video/Source
    Probing devices...

    Device found:

    name : vi-output, tevs 9-003d
    class : Video/Source
    caps : video/x-raw, format=UYVY, width=640, height=480, framerate=60/1
    video/x-raw, format=UYVY, width=1280, height=720, framerate=60/1
    video/x-raw, format=UYVY, width=1280, height=800, framerate=60/1
    video/x-raw, format=NV16, width=640, height=480, framerate=60/1
    video/x-raw, format=NV16, width=1280, height=720, framerate=60/1
    video/x-raw, format=NV16, width=1280, height=800, framerate=60/1
    video/x-raw, format=UYVY, width=640, height=480, framerate=60/1
    video/x-raw, format=UYVY, width=1280, height=720, framerate=60/1
    video/x-raw, format=UYVY, width=1280, height=800, framerate=60/1
    properties:
    object.path = v4l2:/dev/video0
    device.api = v4l2
    media.class = Video/Source
    api.v4l2.path = /dev/video0
    api.v4l2.cap.driver = tegra-video
    api.v4l2.cap.card = "vi-output\,\ tevs\ 9-003d"
    api.v4l2.cap.bus_info = platform:tegra-capture-vi:0
    api.v4l2.cap.version = 5.15.148
    api.v4l2.cap.capabilities = 84200001
    api.v4l2.cap.device-caps = 04200001
    device.id = 33
    node.name = v4l2_input.platform-tegra-capture-vi
    node.description = "vi-output\,\ tevs\ 9-003d"
    factory.name = api.v4l2.source
    node.pause-on-idle = false
    factory.id = 10
    client.id = 32
    clock.quantum-limit = 8192
    media.role = Camera
    node.driver = true
    object.id = 34
    object.serial = 34
    gst-launch-1.0 pipewiresrc path=34 ! ...

    ...

  2. Use the Gstreamer pipeline to launch a 1280x720 resolution camera (/dev/video0) via the CPU:

    $ DISPLAY=:0 gst-launch-1.0 v4l2src device=/dev/video0 ! \
    "video/x-raw, format=UYVY, width=1280, height=720" ! xvimagesink sync=false
  3. Use the Gstreamer pipeline to launch a 1280x720 resolution camera (/dev/video0) via the GPU:

    $ DISPLAY=:0 gst-launch-1.0 nvv4l2camerasrc device=/dev/video0 ! \
    "video/x-raw(memory:NVMM), format=UYVY, width=1280, height=720" ! \
    nvvidconv ! nv3dsink sync=false

Troubleshooting​

Cannot find cameras​

If you cannot bring up the cameras, you can check if the video device does exist.

$ ls /dev/video*  # List all video devices
/dev/video0 /dev/video1

If you cannot see the devices, you should check if the drivers have been probed.

Occur Error: Could not get EGL display connection​

If you occurred the errors nvbufsurftransform: Could not get EGL display connection by rununing the Gstreamer command, you can modify the parameter DISPLAY by the command:

# Check and Set environment parameter for 'DISPLAY'
$ export DISPLAY=$(w| tr -s ' '| cut -d ' ' -f 3 | grep :)

# Run Gstreamer pipeline
$ gst-launch-1.0 v4l2src device=/dev/video0 ! \
"video/x-raw, format=UYVY, width=1280, height=720" ! xvimagesink sync=false

no element "nvv4l2camerasrc"​

If you encounter the following error:

WARNING: erroneous pipeline: no element "nvv4l2camerasrc"

This means your system is missing some NVIDIA GPU-related plug-in tools. You have to install some NVIDIA plug-in tools for Gstreamer.

$ sudo apt update && apt depends nvidia-jetpack | awk '{print $2}' | uniq | xargs -I {} bash -c "sudo apt -o Dpkg::Options::="--force-confold" -y install {} ; sudo apt clean"