CAN Bus
Introduction
This article shows how to set up a CAN network between two boards. This assumes you are working with a product which supports CAN such as EDM1-FAIRY (with EDM1-IMX6), or PICO-NYMPH (with PICO-IMX6, PICO-IMX7, or PICO-IMX6UL/ULL).
Board connections
Set up two boards so that they can exchange CAN information.
| Board A | <-> | Board B |
|---|---|---|
| CAN_H | <-> | CAN_H |
| CAN_L | <-> | CAN_L |
| GND | <-> | GND |
Set up CAN on both boards
Initialize and bring up the CAN interface on both boards.
# ip link set can0 up type can bitrate 125000
On board A, start candump in order to show any received CAN data;
# candump can0
On board B, send some data:
# cansend can0 500#1E.10.10