Skip to main content

Use Flexbuild to Build a Debian Docker Image with HW Acceleration

Introduction

This guide demonstrates how to create a Docker image with hardware acceleration capabilities using Flexbuild for NXP platforms. The resulting Docker container can leverage GPU and ML acceleration from the host system.

Prerequisites

  • Docker: Ensure Docker is installed on your development system. Follow the official Docker installation guide for your operating system.
  • Flexbuild: A build system for creating customized Linux distributions for NXP platforms. For detailed setup instructions, refer to the TechNexion documentation.
  • Storage: At least 15GB of free disk space for the build process.
  • System: A Linux-based development host with necessary packages installed.

Option 1: Use TechNexion's pre-built image on the Docker Hub

TechNexion provides ready-to-use Docker images with hardware acceleration support. This is the quickest way to get started.

Step 1: Pull the pre-built image

# Pull the latest TechNexion Debian image with hardware acceleration
docker pull technexion/tn-image-debian-container:trixie_25.12_imx95

Step 2: Run the container with hardware access

docker run -it \
--name technexion-debian \
-v /run/user:/run/user \
-v /usr/share/fonts:/usr/share/fonts \
--device /dev:/dev \
technexion/tn-image-debian-container:trixie_25.12_imx95 bash

Option 2: Build your own Docker image using Flexbuild

If you need a customized Docker image, follow these steps to build it yourself.

Step 1: Set up the build environment

# Navigate to the Flexbuild directory
cd tn_debian_flexbuild

# Source the environment setup script
. setup.env

Step 2: Build the customized Debian rootfs

This sequence creates a Debian root filesystem that includes NXP's Graphics Acceleration Library and Machine Learning Library:

# Generate whole rootfs for build apps
bld rfs -m imx95-edm
# Build required applications
bld apps -m imx95-edm
# Build the base rootfs for container
bld rfs -r debian:container
# Merge applications into the rootfs
bld merge-apps -r debian:container -m imx95-edm
# Package the rootfs for distribution
bld packrfs -r debian:container -m imx95-edm

Step 3: Create a Dockerfile

Navigate to the images directory:

cd build_lsdk2512/images

Create a Dockerfile with the following content:

FROM scratch
ADD rootfs_lsdk2512_debian_container_imx95-edm.tar.zst /
ENV XDG_RUNTIME_DIR=/run/user/0
ENV WAYLAND_DISPLAY=wayland-1
CMD ["/usr/bin/bash"]

Step 4: Build the Docker image

Build the Docker image with the proper architecture specification:

docker buildx build --platform linux/arm64 -t debian-nxp-hw-accel:latest .

Step 5: Save the Docker image as a tar file

docker save debian-nxp-hw-accel:latest -o debian-nxp-hw-accel.tar

Step 6: Deploy to the target board

Transfer the tar file to your NXP-based target board using either USB drive, SSH/SCP, or any other file transfer method:

# Example using scp
scp debian-nxp-hw-accel.tar user@target-board:/home/user/

On the target board, load the Docker image:

docker load -i debian-nxp-hw-accel.tar

Step 7: Run the Docker container with hardware access

docker run -it \
--name debian-hw-accel \
--privileged \
-v /run/user:/run/user \
-v /usr/share/fonts:/usr/share/fonts \
--device /dev:/dev \
debian-nxp-hw-accel:latest bash

Testing Hardware Acceleration

After launching the container, you can verify hardware acceleration is working:

# Run glmark2 to test GPU acceleration
glmark2-es2-wayland

# Run other GPU or ML demos as needed

Suggestion

info

Host yocto system is best to use tn-image-docker or tn-image-podman target image. These are the yocto images after shrinking. With docker image, the host doesn't need to have that complete system.

bitbake tn-image-docker

or

bitbake tn-image-podman

Troubleshooting

  • If GPU acceleration isn't working, verify that device permissions are correctly configured
  • For "Failed to open device" errors, check that the GPU driver is loaded in the host system
  • When encountering network issues during apt operations inside the container, the retry configuration should help

Additional Notes

  • This Docker image retains hardware acceleration capabilities of the host system
  • The container shares the host's device nodes through the --device /dev:/dev parameter
  • For production deployments, consider restricting device access to only required hardware components