Skip to main content

Intel Panther Lake CRB GMSL2 Cameras

Introduction​

This article explains how to enable TechNexion VLS-GM2 Cameras on the Intel Panther Lake CRB platform. It covers the required BIOS, OS, driver, and camera preview configuration for VLS-GM2 Cameras on Intel Panther Lake CRB.

Supported Camera Modules​

Camera SeriesProducts
VLS-GM2
VLS-GM2-AR0144
VLS-GM2-AR0145
VLS-GM2-AR0234
VLS-GM2-AR0235
VLS-GM2-AR0246
VLS-GM2-AR0521
VLS-GM2-AR0522
VLS-GM2-AR0544
VLS-GM2-AR0821
VLS-GM2-AR0822
VLS-GM2-AR0830
VLS-GM2-AR1335
VLS-GM2-AR2020
Camera Sensor Comparison

More Camera Products Details...

Software Installation Instructions​

BIOS Configurations​

Configure the camera settings in the BIOS first. Follow the steps below.

  1. Power on the Intel Panther Lake CRB device and press the F2 key to enter the BIOS setup.

  2. Use the arrow keys to navigate to Intel Advanced Menu -> Power & performance -> CPU - Power Management Control and set C states to Disabled.

  3. Use the arrow keys to navigate to Intel Advanced Menu -> System Agent (SA) Configuration -> MIPI Camera Configuration and set CVF/CVS Support to Disabled.

  4. Use the arrow keys to navigate to Intel Advanced Menu -> System Agent (SA) Configuration -> MIPI Camera Configuration.

  5. Enable Camera 1 and Camera 2 to show Link options.

  6. Set up the Camera 1 and Camera 2 link options according to the tables below.

Camera 1 Link Options

OptionsParameter
Sensor Model<User Custom>
Custom HIDVLSGM296
Lanes Clock division<4 4 2 2>
CRD Version<CRD-D>
GPIO control<Control Logic 1>
Camera position<back>
Flash Support<Driver default>
Privacy LED<Driver default>
Rotation<180>
PPR Value[2]
PPR Unit[4]
Camera module nametevs
MIPI port[0]
LaneUsed<x4>
MCLK[19200000]
EEPROM Type<ROM_NONE>
VCM Type<VCM_NONE>
Number of I2C Components[3]
I2C Channel<I2C1>
Device 0
I2C Address[0x27]
Device Type<Sensor>
Device 1
I2C Address[0x44]
Device Type<Sensor>
Device 2
I2C Address[0x54]
Device Type<Sensor>
Customize Device ID List
Customize Device1 ID Number[17]
Customize Device1 ID Number[18]
Customize Device1 ID Number[19]
Flash Driver Selection<Disabled>

Camera 2 Link Options

OptionsParameter
Sensor Model<User Custom>
Custom HIDVLSGM296
Lanes Clock division<4 4 2 2>
CRD Version<CRD-D>
GPIO control<Control Logic 2>
Camera position<back>
Flash Support<Driver default>
Privacy LED<Driver default>
Rotation<0>
Voltage Rail<3 voltage rail>
PPR Value[2]
PPR Unit[4]
Camera module nametevs
MIPI port[2]
LaneUsed<x4>
MCLK[19200000]
EEPROM Type<ROM_NONE>
VCM Type<VCM_NONE>
Number of I2C Components[3]
I2C Channel<I2C2>
Device 0
I2C Address[0x27]
Device Type<Sensor>
Device 1
I2C Address[0x44]
Device Type<Sensor>
Device 2
I2C Address[0x54]
Device Type<Sensor>
Customize Device ID List
Customize Device1 ID Number[17]
Customize Device1 ID Number[18]
Customize Device1 ID Number[19]
Flash Driver Selection<Disabled>

OS Configurations​

Install Ubuntu 24.04. You can download it from the following website.

Download latest LTS Ubuntu 24.04

Camera Drivers Installation​

After installing and setting up Ubuntu 24.04, please follow the steps below to complete the Camera Driver installation.

  1. Download the driver packages to the device. Download DEB Packages You can use the following command to download the packages:
wget https://download.technexion.com/demo_software/EVK/Intel/PTL/release/tn-camera-ptl.tar.gz
  1. Next, extract the file and run the install.sh script to install the camera driver packages.
tar xf tn-camera-ptl.tar.gz && sudo ./tn-camera-ptl/install.sh
  1. After installation is complete, reboot the device and verify the installed kernel version.
$ uname -r
6.17.0-tn-ptl-260128t080735z

Enable Cameras​

Use the test script to enable cameras.

vlsgm2-1 through vlsgm2-4 are assigned by the deserializer to port 0. vlsgm2-5 through vlsgm2-8 are assigned by the deserializer to port 2.

For example:

  1. Enable a single sensor:
launch_video_pipeline_ptl.sh vlsgm2-1 1280x720 UYVY
launch_video_pipeline_ptl.sh vlsgm2-5 1280x720 UYVY
  1. Enable all sensors on one port:
launch_video_pipeline_ptl.sh MULTICAMx4-CSI0 1920x1080 UYVY
launch_video_pipeline_ptl.sh MULTICAMx4-CSI2 1920x1080 UYVY
  1. Enable all sensors on both ports:
launch_video_pipeline_ptl.sh MULTICAMx8 640x480 UYVY