PICO-IMX8M-MINI-Boot-Configurations
Boot Configuration Settings: PICO-IMX8M-MINI
Settings for PICO-PI Baseboard
Below is a picture representation of the boot configuration jumper settings for PICO-IMX8M-MINI on our PICO-PI baseboard. Configure the jumpers according to the boot selection you need.
There are two main boot configuration settings: Boot from EMMC, and Serial Download Mode. There is also an option to boot from MicroSD card on PICO-PI, via the included CLIX SD card adapter.
- Note that on PICO-IMX8M-MINI, the default boot media is EMMC. On the module, we configure boot configuration signals to boot from the default media without needing to be pulled high or low on the baseboard. You can either leave the jumpers as set here, or remove them.
In serial download mode, the PICO-IMX8M-MINI will look for commands to be sent to it over USB OTG. This is used to load new software onto the unit.
To boot from SD card, please set the jumpers according to the picture below:
Settings for PICO-WIZARD Baseboard
To boot from the module e.MMC, set the boot jumpers as below:
To Boot into Serial Download Mode, set the jumpers as below:
To boot from SD card, please set the jumpers according to the picture below: