AXON-heatsink-installation-guide
Installing the TechNexion low-profile AXON heatsink
The following steps and picture describe how to install the TechNexion heatsink onto an AXON module (AXON-E-IMX8M-PLUS, or AXON-IMX8M-MINI).
1. Prepare your AXON baseboard, AXON module, wireless antenna (if applicable) and AXON heatsink kit. Besides this, you need the following tools: A hexagonal 3.0 x 7.5 sleeve screwdriver and a pincer (tweezers).
2. Locate four mounting holes on the baseboard (these are 4 soldered standoffs). Align module with the holes and baseboard connectors, and gently press into the development board to secure it. Press on the mounting holes and directly above the board to board connectors. Do not press in the center of the module. You will hear an audible click sound as the connectors are mated.
Note: When pressing the module down onto the baseboard connectors, do NOT press into the center of the module. This can cause the module PCB to flex and can cause cracking in the solder joints.
3. Place heat sink thermal pads on the applications processor and wireless module, and also install the provided mylar sticker on the heat sink bottom of the heat sink.
Note: The mylar sticker prevents the antenna connector from contacting the underside of the heatsink, and also helps to ensure that that connector stays in place.
4. Locate the MHF4 wireless antenna connector on the module. Align the small round MHF4 connector at the end of the antenna cable onto this connector. Once aligned, will need to press down on the antenna cable connector until you hear a click sound.
5. Insert 4x dual-threaded hex screws (provided) into the holes and tighten.
6. Insert slowly the heat sink and gently press into the development board. Then secure the heatsink with 4 hex nuts (provided).
Note: Do not power your board during the installation process