Installation
  • 18 Apr 2025
  • 2 Minutes to read
  • Dark
    Light
  • PDF

Installation

  • Dark
    Light
  • PDF

Article summary

Installation VizionViewer™

Windows-x64

  1. Download the VizionViewer™ installer for Windows.
  2. Once it is downloaded, run the installer (vizionviewersetup_{version}.exe).
  3. By default, VizionViewer™ is installed under C:\Program Files\VizionViewer.

Linux-x64

Support Platform:

  • General PCs (Ubuntu Desktop 20.04, Ubuntu 22.04)
  • UP Squared Pro 7000

Offline Installation

  1. Download the .deb packages for Ubuntu.
  2. uncompress and install .deb packages, You can do this either through the graphical software center if available or via the command line using:
tar -xf ./vizionviewersetup_{version}_linux64.tar.xz
sudo apt install ./vizionsdk.deb
sudo apt install ./vizionviewer.deb
  1. Installing the .deb package will automatically install the apt repository and signing key to enable auto-updating using the system's package manager.

Online Installation

The repository and key can also be installed manually with the following script:

sudo apt-get install wget gpg
wget -qO- https://download.technexion.com/apt/technexion.asc | gpg --dearmor > packages.technexion.gpg
sudo install -D -o root -g root -m 644 packages.technexion.gpg /etc/apt/keyrings/packages.technexion.gpg
sudo sh -c 'echo "deb [arch=amd64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionsdk/ stable main" > /etc/apt/sources.list.d/vizionsdk.list'
sudo sh -c 'echo "deb [arch=amd64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionviewer/ stable main" >> /etc/apt/sources.list.d/vizionsdk.list'

Then update the package cache and install the package using:

sudo apt update
sudo apt install vizionsdk vizionviewer

When using UP Squared Pro 7000, please add Gstreamer library to environment:

export GST_PLUGIN_PATH=/usr/lib/gstreamer-1.0

Linux-ARM64

Requirements:

  • GCC >= 11.5 and glibc >= 2.35

Support Platform:

  • NVIDIA Jetson (JetPack 6.x or later)
  • NXP-i.MX8MM, NXP-i.MX8MQ, NXP-i.MX8MP, NXP-i.MX93, NXP-i.MX95
  • TI-TDA4VM

Offline Installation

  1. Download the .deb packages for Linux-ARM.
  2. uncompress and install .deb packages, You can do this either through the graphical software center if available or via the command line using:
tar -xf ./vizionviewersetup_{version}_linuxarm64.tar.xz
sudo apt install ./vizionsdk.deb
sudo apt install ./vizionviewer.deb
  1. Installing the .deb package will automatically install the apt repository and signing key to enable auto-updating using the system's package manager.

Online Installation

The repository and key can also be installed manually with the following script:

sudo apt-get install wget gpg
wget -qO- https://download.technexion.com/apt/technexion.asc | gpg --dearmor > packages.technexion.gpg
sudo install -D -o root -g root -m 644 packages.technexion.gpg /etc/apt/keyrings/packages.technexion.gpg
sudo sh -c 'echo "deb [arch=arm64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionsdk/ stable main" > /etc/apt/sources.list.d/vizionsdk.list'
sudo sh -c 'echo "deb [arch=arm64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionviewer/ stable main" >> /etc/apt/sources.list.d/vizionsdk.list'

Then update the package cache and install the package using:

sudo apt update
sudo apt install vizionsdk vizionviewer

Troubleshooting & Migration Notes

Toolchain Compatibility

⚠️ Platforms with older toolchains (e.g., GCC < 11 or glibc < 2.34) are not supported in the current release.
If you are using Jetpack 4.x or Jetpack 5.x, please refer to the VizionViewer Release Note for a compatible version.

Deprecated APT Repository

⚠️ The stable jetson APT repository has been deprecated.
Please use the stable main repository instead, as shown in Online Installation.


Was this article helpful?

What's Next