- 24 Apr 2025
- 1 Minute to read
- Print
- DarkLight
- PDF
Installation
- Updated on 24 Apr 2025
- 1 Minute to read
- Print
- DarkLight
- PDF
Supported Python Versions
The pyvizionsdk package is built as a CPython extension. The package enhances performance using CPython’s extension mechanisms while maintaining compatibility with Python’s ecosystem.
Python 3.8
Python 3.9
Python 3.10
Python 3.11
Python 3.12
Python 3.13
How to install pyvizionsdk
Windows-x64
Download the
.whl
file and usepip
to install wheel fileDownload the pyvizionsdk for Windows: pyvizionsdk Download Page.
Download the wheel file with Python version on your device:
pyvizionsdk-{version}-cp{python_version}-cp{python_version}-win_amd64.whl
Open Command Prompt or PowerShell
Install the pyvizionsdk using
pip
:pip install pyvizionsdk-{version}-cp{python_version}-cp{python_version}-win_amd64.whl
pip install
from the website directlypip install pyvizionsdk --extra-index-url https://pypi.vizionsdk.com/root/pyvizionsdk/+simple/
Linux-x64
Supported platforms
General PCs, UP Squared Pro 7000
Installation
Download the
.whl
file and usepip
to install wheel fileDownload the pyvizionsdk for Linux: pyvizionsdk Download Page.
Download the wheel file with Python version on your device:
pyvizionsdk-{version}-cp{python_version}-cp{python_version}-manylinux_2_31_x86_64.whl
Open Command Prompt or PowerShell
Install the pyvizionsdk using
pip
:pip install pyvizionsdk-{version}-cp{python_version}-cp{python_version}-manylinux_2_31_x86_64.whl
pip install
from the website directlypip install pyvizionsdk --extra-index-url https://pypi.vizionsdk.com/root/pyvizionsdk/+simple/
Linux-ARM64
Supported platforms
NXP-iMX8MP, NXP-iMX8MM, NXP-iMX93, NXP-iMX95
NVIDIA-Jetpack5.x and Later
Installation
Download the
.whl
file and usepip
to install wheel fileDownload the pyvizionsdk for ARM: pyvizionsdk Download Page.
Download the wheel file with Python version on your device:
pyvizionsdk-{version}-cp{python_version}-cp{python_version}-manylinux_2_34_aarch64.whl
Open Command Prompt or PowerShell
Install the pyvizionsdk using
pip
:pip install pyvizionsdk-{version}-cp{python_version}-cp{python_version}-manylinux_2_34_aarch64.whl
pip install
from the website directlypip install pyvizionsdk --extra-index-url https://pypi.vizionsdk.com/root/pyvizionsdk/+simple/
Configuration Setup
After installing, the VxConfig.conf will set up in the following path.
Windows:
C:\Users\{UserName}\AppData\Local\Programs\Python{version}\Lib\site-packages\pyvizionsdk\VxConfig.conf
Linux, NXP-iMX, NVIDIA-Jetpack5.x and Later:
~/.local/lib/python{version}/site-packages/pyvizionsdk/VxConfig.conf
The config file is for pyvizionsdk to recognize the device, which is TechNexion series camera.
The location of VxConfig.conf can be customized by setting the VIZIONSDK_CONFIG_PATH environment variable.Import the library
Import the pyvizionsdk library and start to use the pyvizionsdk
import pyvizionsdk
# test the library import success or not
pyvizionsdk.HelloVizionSDK()
# Hello VizionSDK!
# Version: {VizionSDK Version}