- 15 May 2025
- 2 Minutes to read
- Print
- DarkLight
- PDF
Use Flexbuild to Build a Debian Docker Image with HW Acceleration
- Updated on 15 May 2025
- 2 Minutes to read
- Print
- DarkLight
- PDF
Introduction
This guide demonstrates how to create a Docker image with hardware acceleration capabilities using Flexbuild for NXP platforms. The resulting Docker container can leverage GPU and ML acceleration from the host system.
Prerequisites
- Docker: Ensure Docker is installed on your development system. Follow the official Docker installation guide for your operating system.
- Flexbuild: A build system for creating customized Linux distributions for NXP platforms. For detailed setup instructions, refer to the TechNexion documentation.
- Storage: At least 15GB of free disk space for the build process.
- System: A Linux-based development host with necessary packages installed.
Option 1: Use TechNexion's pre-built image on the Docker Hub
TechNexion provides ready-to-use Docker images with hardware acceleration support. This is the quickest way to get started.
Step 1: Pull the pre-built image
# Pull the latest TechNexion Debian image with hardware acceleration
docker pull technexion/tn-image-debian-container:bookworm_24.12
Step 2: Run the container with hardware access
docker run -it \
--name technexion-debian \
-v /run/user:/run/user \
-v /usr/share/fonts:/usr/share/fonts \
--device /dev:/dev \
technexion/tn-image-debian-container:bookworm_24.12 bash
Option 2: Build your own Docker image using Flexbuild
If you need a customized Docker image, follow these steps to build it yourself.
Step 1: Set up the build environment
# Navigate to the Flexbuild directory
cd tn_debian_flexbuild
# Source the environment setup script
. setup.env
Step 2: Build the customized Debian rootfs
This sequence creates a Debian root filesystem that includes NXP's Graphics Acceleration Library and Machine Learning Library:
# Build the base rootfs
bld rfs -p IMX -f tn_technexion.yml
# Build required applications
bld apps -p IMX -f tn_technexion.yml
# Merge applications into the rootfs
bld merge-apps -p IMX -f tn_technexion.yml
# Package the rootfs for distribution
bld packrfs -p IMX -f tn_technexion.yml
Step 3: Create a Dockerfile
Navigate to the images directory:
cd build_lsdk2412/images
Create a Dockerfile with the following content:
FROM scratch
ADD rootfs_lsdk2412_debian_desktop_arm64.tar.zst /
ENV XDG_RUNTIME_DIR=/run/user/0
ENV WAYLAND_DISPLAY=wayland-1
CMD ["/usr/bin/bash"]
Step 4: Build the Docker image
Build the Docker image with the proper architecture specification:
docker buildx build --platform linux/arm64 -t debian-nxp-hw-accel:latest .
Step 5: Save the Docker image as a tar file
docker save debian-nxp-hw-accel:latest -o debian-nxp-hw-accel.tar
Step 6: Deploy to the target board
Transfer the tar file to your NXP-based target board using either USB drive, SSH/SCP, or any other file transfer method:
# Example using scp
scp debian-nxp-hw-accel.tar user@target-board:/home/user/
On the target board, load the Docker image:
docker load -i debian-nxp-hw-accel.tar
Step 7: Run the Docker container with hardware access
docker run -it \
--name debian-hw-accel \
-v /run/user:/run/user \
-v /usr/share/fonts:/usr/share/fonts \
--device /dev:/dev \
debian-nxp-hw-accel:latest bash
Testing Hardware Acceleration
After launching the container, you can verify hardware acceleration is working:
# Run glmark2 to test GPU acceleration
glmark2-es2-wayland
# Run other GPU or ML demos as needed
Suggestion
Host yocto system is best to use tn-image-docker
or tn-image-podman
target image. These are the yocto images after shrinking. With docker image, the host doesn't need to have that complete system.
bitbake tn-image-docker
or
bitbake tn-image-podman
Troubleshooting
- If GPU acceleration isn't working, verify that device permissions are correctly configured
- For "Failed to open device" errors, check that the GPU driver is loaded in the host system
- When encountering network issues during apt operations inside the container, the retry configuration should help
Additional Notes
- This Docker image retains hardware acceleration capabilities of the host system
- The container shares the host's device nodes through the
--device /dev:/dev
parameter - For production deployments, consider restricting device access to only required hardware components