- 24 Mar 2025
- 5 Minutes to read
- Print
- DarkLight
- PDF
TI BeaglePlay TEVS Camera Usage Guide
- Updated on 24 Mar 2025
- 5 Minutes to read
- Print
- DarkLight
- PDF
Introduction
TechNexion Embedded Vision Solutions provide embedded system developers access to high-performance, industrial-grade camera solutions to accelerate their time to market for embedded vision projects.
Support Camera Modules
Camera Series | Products |
---|---|
TEVS | TEVS-AR0144 |
More Camera Products Details...
Support System Version
Supported TI Development Kit
Install TN Camera on TI Development Kit
Adaptor for BeaglePlay
TEVS-RPI22 Adaptor for TEVS
Connect TEVS camera and TEVS-RPI22 adaptor to BeaglePlay - CSI directly.
Method 1 - Using Technexion Pre-built modules, only for kernel 6.6.32-ti-arm64-r7
Make a SD card with "BeaglePlay Debian 12.6 2024-07-04 XFCE" image.
Mount boot partition and configure sysconf.txt before the first boot.
$ vim /media/${user}/BOOT/sysconf.txt
> # root_password - Set a password for the root user (not used in ubuntu)
> root_password=root
>
> # user_name - Set a user name for the user (1000)
> user_name=beagle
>
> # user_password - Set a password for user (1000)
> user_password=beagle
Boot BeaglePlay with SD card.
Download pre-built modules.
$ wget https://download.technexion.com/demo_software/EVK/TI/BeaglePlay/pre-built-modules/latest/tn_camera_module_beagleplay_6.6.32.tar.gz
Uncompress the modules.
$ tar -xf tn_camera_module_beagleplay_6.6.32.tar.gz
Run installation script.
$ cd tn_camera_module_beagleplay_6.6.32/
$ sh tn_install.sh
[sudo] password for beagle:
****** TechNexion Camera Driver Installation ******
This installation is easy to install TechnNexion Camera Drivers for BeaglePlay.
Before start to install camera driver, You should BACKUP your image and config
to avoid any file you lost while installing process.
Do you want to continue?[Y/n]y
Continuing with the installation...
Install TN-CAM modules: tevs.ko.xz
Installed TN-CAM module file Done.
Install TN-CAM DTBO file: k3-am625-beagleplay-csi2-tevs-rpi22.dtbo
Installed TN-CAM DTBO file Done.
Add TN-CAM Configuration for modules: tevs-rpi22
label microSD (default)
Install TN-CAM service...
Launch TN-CAM Service...
Created symlink /etc/systemd/system/multi-user.target.wants/tn_cam.service → /etc/systemd/system/tn_cam.service.
Finish Camera Driver Installation. Return Code:[1]
You should Reboot Device to enable TEVS Cameras.
Do you want to reboot now?[Y/n]y
Rebooting....
Method 2 - Build drivers from source code (cross-compiling)
You can reference BeagleBone Cookbook - The Kernel.
Make sure the dependencies.
$ sudo apt install -y git bc bison flex libssl-dev make libc6-dev libncurses5-dev
# Install the 64-bit toolchain for a 64-bit kernel
$ sudo apt install -y crossbuild-essential-arm64
Get the kernel sources.
# beagleboard linux kerbel
$ git clone --depth=1 -b v6.6.32-ti-arm64-r7 https://github.com/beagleboard/linux.git
# technexion beagle camera driver
$ git clone --depth=1 -b v6.6.32-ti-arm64 https://github.com/TechNexion-Vision/beagle_devkit_camera_driver.git
Copy TN beagle camera driver to beagleboard linux kernel.
$ cp -rv beagle_devkit_camera_driver/drivers/media/i2c/* linux/drivers/media/i2c/
$ cp -rv beagle_devkit_camera_driver/arch/arm64/boot/dts/ti/* linux/arch/arm64/boot/dts/ti/
Build sources.
$ cd linux
# default configuration
$ make distclean
$ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- olddefconfig
# config camera
$ make menuconfig
# -> Device Drivers
# -> Multimedia support (MEDIA_SUPPORT [=m])
# -> Media ancillary drivers
# -> Camera sensor devices (VIDEO_CAMERA_SENSOR [=y])
# -> TechNexion TEVS sensor support
# Set "VIDEO_TEVS" to module,
# Press "m", save to original name (.config) and exit
# build kernel
$ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- LOCALVERSION="-tn-arm64" -j$(nproc)
$ mkdir -p modules
$ sudo make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- INSTALL_MOD_PATH=./modules modules_install
Plug in the SD card which burned "BeaglePlay Debian 12.6 2024-07-04 XFCE" image to PC.
Configure sysconf.txt before the first boot.
$ vim /media/${user}/BOOT/sysconf.txt
> # root_password - Set a password for the root user (not used in ubuntu)
> root_password=root
>
> # user_name - Set a user name for the user (1000)
> user_name=beagle
>
> # user_password - Set a password for user (1000)
> user_password=beagle
Install onto the SD card.
$ sudo cp arch/arm64/boot/Image /media/$(users)/BOOT/
$ sudo cp arch/arm64/boot/dts/ti/*.dtbo /media/$(users)/BOOT/overlays/
# you can use "make kernelversion" to check kernel version
$ sudo cp -ra modules/lib/modules/$(make kernelversion)-tn-$(git_commit)-dirty/ /media/$(users)/rootfs/lib/modules/
$ sync
Boot BeaglePlay with SD card.
Modify the extlinux.conf file to add camera configuraion.
$ sudo nano /boot/firmware/extlinux/extlinux.conf
> label microSD (default)
> kernel /Image
> append root=/dev/mmcblk1p3 ro rootfstype=ext4 resume=/dev/mmcblk1p2 rootwait net.ifnames=0 quiet
> fdtdir /
> fdtoverlays /overlays/k3-am625-beagleplay-csi2-tevs-rpi22.dtbo
> initrd /initrd.img
Add the overlay to label microSD (default)
and append fdtoverlays /overlays/k3-am625-beagleplay-csi2-tevs-rpi22.dtbo
after the fdtdir
line.
Restart system.
$ sudo reboot
Bring up Camera by GStreamer
If you succeed in initialing the camera, you can follow the steps to open the camera.
Check the media deivce.
$ media-ctl -d /dev/media0 -p
Device topology
- entity 1: 30102000.ticsi2rx (5 pads, 5 links)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
pad0: Sink
[fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
- entity 7: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
[fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "tevs 4-0048":0 [ENABLED,IMMUTABLE]
pad1: Source
[fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
pad3: Source
pad4: Source
- entity 13: tevs 4-0048 (1 pad, 1 link)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev2
pad0: Source
[fmt:UYVY8_1X16/640x480@1/60 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/640x480
crop:(0,0)/640x480]
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
- entity 19: 30102000.ticsi2rx context 0 (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: Sink
<- "30102000.ticsi2rx":1 [ENABLED,IMMUTABLE]
...
List device support formats and resolutions.
# list support format
$ v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-mbus-codes
> ioctl: VIDIOC_SUBDEV_ENUM_MBUS_CODE (pad=0)
> 0x200f: MEDIA_BUS_FMT_UYVY8_1X16
# list support frame size with format
$ v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-framesize code=0x200f
> ioctl: VIDIOC_SUBDEV_ENUM_FRAME_SIZE (pad=0)
> Size Range: 640x480 - 640x480
> Size Range: 1280x720 - 1280x720
> Size Range: 1280x800 - 1280x800
# list support frame intercal with format and resolution
$ v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-frameintervals \
pad=0,width=1280,height=720,code=0x2006
> ioctl: VIDIOC_SUBDEV_ENUM_FRAME_INTERVAL (pad=0)
> Interval: 0.017s (60.000 fps)
Bring up the camera (/dev/video0) with 640x480 by Gstreamer pipeline.
$ DISPLAY=:0 gst-launch-1.0 v4l2src device=/dev/video0 ! \
"video/x-raw, format=UYVY, width=640, height=480" ! fpsdisplaysink sync=false
Change resolution with 1280x720 and bring up by Gstreamer pipeline directly.
# modify media resoltion
media-ctl -V '"tevs 4-0048":0 [fmt:UYVY8_1X16/1280x720]'
media-ctl -V '"30102000.ticsi2rx":0 [fmt:UYVY8_1X16/1280x720]'
$ DISPLAY=:0 gst-launch-1.0 v4l2src device=/dev/video0 ! \
"video/x-raw, format=(string)UYVY, width=(int)1280, height=(int)720" ! \
fpsdisplaysink video-sink=glimagesink sync=false