- 11 Apr 2025
- 2 Minutes to read
- Print
- DarkLight
- PDF
Installation
- Updated on 11 Apr 2025
- 2 Minutes to read
- Print
- DarkLight
- PDF
How to install VizionSDK
Windows
Download the VizionSDK for Windows from the following link: VizionSDK Download Page.
Once downloaded, run the installer (vizionsdk-{version}-win64.exe).
By default, VizionSDK is installed under C:\Program Files\vizionsdk
Linux
Supported platforms
General PCs, UP Squared Pro 7000
Offline Installation
Download the VizionSDK .deb packages for Ubuntu from the following link: VizionSDK .deb packages Download Page.
Uncompress
.tar
folder and you can link to the local librarytar -xf ./vizionsdk-{version}-linux64.tar
Install
.deb
packages. You can do this either through the graphical software center if available or via the command line using:sudo apt install ./vizionsdk-linux64.deb
Installing the .deb package will automatically install the apt repository and signing key to enable auto-updating using the system's package manager.
Online Installation
The repository and key can also be installed manually with the following script:
sudo apt-get install wget gpg wget -qO- https://download.technexion.com/apt/technexion.asc | gpg --dearmor > packages.technexion.gpg sudo install -D -o root -g root -m 644 packages.technexion.gpg /etc/apt/keyrings/packages.technexion.gpg sudo sh -c 'echo "deb [arch=amd64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionsdk/ stable main" > /etc/apt/sources.list.d/vizionsdk.list' sudo sh -c 'echo "deb [arch=amd64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionviewer/ stable main" >> /etc/apt/sources.list.d/vizionsdk.list'
Then update the package cache and install the package using:
sudo apt update sudo apt install vizionsdk
ARM
Supported platforms
NXP-iMX8MP, NXP-iMX8MM, NXP-iMX93, NXP-iMX95
NVIDIA-Jetpack5.x and Later
Offline Installation
Download the VizionSDK .deb packages for ARM from the following link: VizionSDK .deb packages Download Page.
Uncompress
.tar
folder and you can link to the local librarytar -xf ./vizionsdk-{version}-linuxarm64.tar
Install
.deb
packages. You can do this either through the graphical software center if available or via the command line using:sudo apt install ./vizionsdk-linuxarm64.deb
Installing the .deb package will automatically install the apt repository and signing key to enable auto-updating using the system's package manager.
Online Installation
The repository and key can also be installed manually with the following script:
For Jetpack user, the stable main version is different from the legacy stable version.
sudo apt-get install wget gpg wget -qO- https://download.technexion.com/apt/technexion.asc | gpg --dearmor > packages.technexion.gpg sudo install -D -o root -g root -m 644 packages.technexion.gpg /etc/apt/keyrings/packages.technexion.gpg sudo sh -c 'echo "deb [arch=arm64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionsdk/ stable main" > /etc/apt/sources.list.d/vizionsdk.list' sudo sh -c 'echo "deb [arch=arm64 signed-by=/etc/apt/keyrings/packages.technexion.gpg] https://download.technexion.com/apt/vizionviewer/ stable main" >> /etc/apt/sources.list.d/vizionsdk.list'
Then update the package cache and install the package using:
sudo apt update sudo apt install vizionsdk
Configuration Setup
After installing, the VxConfig.conf will setup in the following path.
Windows:
C:\Program Files\vizionsdk\bin\VxConfig.conf
Linux, NXP-iMX, NVIDIA-Jetpack5.x and Later:
/usr/share/vizionsdk/VxConfig.conf
Local library:
/vizionsdk-{version}-{os}/bin/VxConfig.conf
The config file is for VizionSDK to recognize the device which is TechNexion series camera.
The location of VxConfig.conf can be customized by setting the VIZIONSDK_CONFIG_PATH environment variable.
How to use VizionSDK
There is the example for linking the VizionSDK library by CMake.
You can follow the steps in Sample Build Guide to install the necessary package in your host PC.
Prerequisites
CMake (version 3.0 or newer)
C++ compiler
Import the library
Include the VizionSDK header file in the code
#include "VizionSDK.h"
Build the project with CMake
Link the library from installation (.exe, .deb or apt install)
Using CMake to find the package and link VizionSDK library.
# Find VizionSDK package
find_package(vizionsdk REQUIRED)
# Add executable
add_executable({PROJECT_NAME}
{project}.cpp
)
# Link libraries
target_link_libraries({PROJECT_NAME}
PRIVATE
vizionsdk::VizionSDK
)
Link the library from local folder
Link the library which is located in the local folder ../Downloads/vizionsdk-{version}-{arch}/lib
.
# Set path to the SDK library directory
# NOTE: Update this path to match your SDK location
target_link_directories({PROJECT_NAME}
PRIVATE
${CMAKE_CURRENT_SOURCE_DIR}/../../Downloads/vizionsdk-{version}-{arch}/lib
)
# Link libraries
target_link_libraries({PROJECT_NAME}
PRIVATE
VizionSDK
)