Building Sample Code for VizionSDK
  • 25 Sep 2024
  • 2 Minutes to read
  • Dark
    Light
  • PDF

Building Sample Code for VizionSDK

  • Dark
    Light
  • PDF

Article summary

Introduction

This article will explain how to build sample code for VizionSDK.
You can download the Sample code here.

Prerequisites

Before building and running this project, ensure you have the following installed:

CMake (version 3.0 or newer)

  • Windows:

    • You can download the latest CMake installer from the official CMake website and follow the installation instructions provided.
    • Ensure that CMake is added to your system PATH during installation to enable command-line usage.
  • Linux:

    • On Debian-based systems (e.g., Ubuntu), you can install CMake using apt:

      sudo apt update
      sudo apt install cmake
      
    • If sudo apt install cmake is not available. You can manually download and install CMake from the official website:

      If you're working with NXP, Nvidia, or TI platforms look for the Linux aarch64 binary distribution. Download the appropriate tar.gz file for your platform.

      1. Extract the downloaded file:
      tar -zxvf cmake-[version]-linux-aarch64.tar.gz
      
      1. Move the extracted directory:
        • Move the extracted files to a directory like /opt for easier management:
          sudo mv cmake-[version]-linux-aarch64 /opt/cmake
          
      2. Update the PATH environment variable:
        • Add CMake to your system PATH by modifying your ~/.bashrc or ~/.profile file:
           export PATH=/opt/cmake/bin:$PATH
          
        • Save the file and reload your profile with
           source ~/.profile
          

    C++ compiler (supporting C++11 standard)

  • Windows:

    • For Windows, you might need to install a C++ compiler separately. You can use Microsoft Visual Studio, which includes the MSVC compiler.
      • When installing Visual Studio, make sure to select the "Desktop development with C++" workload during the installation process. This will include the necessary C++ compiler, nmake, and other essential tools for C++ development on Windows.
    • Alternatively, you can use MinGW, a port of the GNU Compiler Collection (GCC), which provides a C++ compiler for Windows.
  • Linux:

    • Most Linux distributions come with a C++ compiler pre-installed. However, if it's not available, you can install it using your package manager.
      On Debian-based systems (e.g., Ubuntu), you can install the GNU Compiler Collection (GCC) using apt:
      sudo apt update
      sudo apt install build-essential
      
    • Embedded systems:
      Embedded systems typically do not require a compiler. Development is done using cross-compilation on a host machine, and the resulting binaries are deployed to the embedded device.

    Building

Windows

  1. Open Command Prompt or PowerShell.
  2. Navigate to the Samples directory of the project:
  3. Create a build directory: mkdir build && cd build
  4. Generate build files using CMake (replace your_platform with Windows, Ubuntu, IMX, TI, or Nvidia):
cmake -DPLATFORM=[your_platform] ..
  1. Build the project using the generated build files: cmake --build . --config Release

Linux

  1. Open Terminal.
  2. Navigate to the Samples directory of the project:
  3. Create a build directory: mkdir build && cd build
  4. Generate build files using CMake (replace your_platform with Windows, Ubuntu, IMX, TI, or Nvidia):
cmake -DPLATFORM=[your_platform] ..
  1. Build the project using the generated build files: make

Running

Windows

  • After successful building, you will find the executable VizionSample.exe in the build directory. You can run it from the command line or by double-clicking on it in the File Explorer.
  • Ensure that you also copy the VizionSDK.dll file next to the executable VizionSample.exe. This DLL file is required for the proper execution of the application.

Linux

  • After successful building, you will find the executable VizionSample in the build directory. Before running it, navigate to the SDK directory in the terminal using cd path_to_sdk, then execute sudo cp VizionSDK.so* /usr/lib/ to copy the necessary SDK files to the system's library directory.
  • After successful building, you will find the executable VizionSample in the build directory. You can run it from the terminal by executing ./VizionSample.

Was this article helpful?