Boot Configurations
- 01 Oct 2021
- 1 Minute to read
- Print
- DarkLight
- PDF
Boot Configurations
- Updated on 01 Oct 2021
- 1 Minute to read
- Print
- DarkLight
- PDF
Article Summary
Share feedback
Thanks for sharing your feedback!
Boot Configurations
The Boot Configuration DIP switch (SW1) is used to control the boot media (e.MMC or microSD card) and is also used to put the module into serial download mode.
Location of Boot Configuration Switch SW1 (Switch is covered in Kapton tape and in OFF position)
Boot Mode | Switch Positions | SW1 Picture |
---|---|---|
Boot from module e.MMC | Both OFF | |
Boot from AXON-PI MicroSD. Requires a loaded bootable microSD card loaded into microSD slot on AXON-PI | 1: ON, 2: OFF | |
Boot into Serial Download Mode | 1: Don't Care, 2: ON |
Was this article helpful?