Introduction
  • 01 Oct 2021
  • 1 Minute to read
  • Dark
    Light
  • PDF

Introduction

  • Dark
    Light
  • PDF

Article summary

About AXON-PI

AXON-PI is a small development baseboard for the AXON series of system on modules a 'Raspberry Pi' form-factor.

Board Pictures

Back View, With Module and Heatsink
axon-pi-imx8m-mini-back-cropped.png

Top View
axon-pi-imx8m-mini-top-cropped.png

Block Diagram

axon-pi-block-diagram.png

Dimensional Drawing

axon-pi-imx8m-mini-dimensions.jpg

Accessories

AXON-PI is compatible with the following additional accessories to enable different use-cases.

Displays

AXON-PI is compatible with a 5" MIPI-DSI (720x1280) portait-mode PCAP touch display with LED backlight. Kits based on AXON-PI (such as AXON-PI-IMX8M-MINI) may be purchased with a 5" display kit included. Datasheets for the display kit can be provided. Please contact your TechNexion sales representative.

HDMI

Kits equipped with AXON-E-IMX8M-PLUS, which supports HDMI 2.0 output up to full HD resolution, can also utilize the HDMI connector on AXON-PI.

Cameras

AXON-PI is compatible with the CAM-OV5645 Camera Kit.

Expansion Boards

AXON-PI is also compatible with the following expansion boards from TechNexion.

VOICEHAT

CLIX Modules


Was this article helpful?