Connectors and Features
- 14 Dec 2021
- 1 Minute to read
- Print
- DarkLight
- PDF
Connectors and Features
- Updated on 14 Dec 2021
- 1 Minute to read
- Print
- DarkLight
- PDF
Article summary
Did you find this summary helpful?
Thank you for your feedback!
Introduction
This article provides you with an overview of the features of the AXON-PI baseboard.
AXON-PI Connectors and Features
Top View
Number | Feature |
---|---|
1 | 40-pin Expansion Connector (see Expansion Connectors) |
2 | User LEDs |
3 | Micro USB Console Connector (On-board USB-UART) |
4 | Camera CSI connector (33-pin FPC) |
5 | CLIX interface GPIO/SDIO Switch Control |
6 | Reset Switch (RESET1) |
7 | USB Type C Connector (OTG) |
8 | User Pushbutton Switch (USER1) |
9 | HDMI Connector (Used with AXON-E-IMX8M-PLUS, not functional with AXON-IMX8M-MINI) |
10 | HDMI Protection IC |
11 | USB 3.0 Switch |
12 | Audio Expansion Connector (see Expansion Connectors) |
13 | 3V RTC Battery Connector |
14 | Touchscreen connector (Used to connect to 5" 720x1280 MIPI-DSI Display Touchscreen) |
15 | MIPI-DSI connector (Used to connect to 5" 720x1280 MIPI-DSI Display) |
16 | Dual USB Type A Connector (AXON-E-IMX8M-PLUS: USB3.0 support, AXON-IMX8M-MINI: USB 2.0 support) |
17 | Gigabit Ethernet RJ45 Jack |
18 | JTAG Connector |
19 | Boot Configuration DIP Switch SW1 (see Boot Configurations) |
20 | Stereo Headphone/Mic Jack |
21 | Stereo Speaker Connectors |
Bottom View
Number | Feature |
---|---|
22 | MicroSD Card Connector |
23 | Wireless Radio and Antenna Connector (On SoM) |
24 | CLIX Expansion Slot (see Expansion Connectors) |
25 | Module LEDs |
26 | AXON System On Module with AXON Heatsink Installed |
Was this article helpful?