Visit TechNexion Website
Contents
x
Products
Software Development
Powered by
Development Guide
7 Articles
in this category
Share this
Print
Share
Dark
Light
Contents
Development Guide
7 Articles
in this category
Share
Dark
Light
Building an Image with Yocto
Introduction This article provides step-by-step instructions for building a Linux image with TechNexion's Yocto BSP, which supports the i.MX series of processors. System Requirements Building an image from source with Yocto requires a host wit...
Updated on : 03 Feb 2025
How to Build Yocto with a Custom Kernel
Follow the steps to build yocto (as described in this page: tn-imx-yocto-manifest ) all the way up to configuring yocto build, before "bitbake" command to start building yocto (The line containing DISTRO=XXX MACHINE=YYY source tn-setup-release....
Updated on : 10 Jul 2023
Build Source Code in Ubuntu Virtual Machine
Introduction The virtual machine is to reduce the complexity of setting up the development environment for building Android, Yocto, and Ubuntu images for TechNexion SOM/baseboards. The virtual machine is based on Ubuntu-20.04 LTS x64 architecture....
Updated on : 01 Oct 2021
Building an Image in Docker Container
Introduction Set up the build environment using container methods. Set up build environment on host PC: The build environment is tested under Ubuntu 22.04. Install required package: $ sudo apt install docker.io Download TechNexion's d...
Updated on : 12 Jun 2023
Tips for Resolving Dependency Issues in Yocto
Introduction A customer of ours recently asked about some problems they were seeing when running an application on a Pico module. They were using Yocto. Many Linux applications, especially Qt applications, require other packages (files, and librar...
Updated on : 01 Oct 2021
Using an NFS Root Filesystem
Introduction NFS (short for Network FileSystem) has been around for a long time. It is an early form of a network file sharing system, where a server can export part of its filesystem so that this can be mounted by a client on the local network. T...
Updated on : 01 Oct 2021
Yocto Project Customization
2 Articles
in this category
Automatically Setting a Root Password in Yocto Recipes
Introduction This article discusses how to set a root password within Yocto metadata so that images are built with a root password included. We show how to do this with both a cleartext password as well as encrypted version of the password. In l...
Updated on : 01 Oct 2021